<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC546xx power lib</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1400136#M47654</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;we are in the process of migrating several projects to LPC546xx devices. Most of those projects do not use short enum/wchar compile options and are therefore not compatible with the compile settings of the provided power lib for Keil.&lt;/P&gt;&lt;P&gt;Can you please provide us with a version compiled without the short enum/wchar option, or is it possible to circumvent using this library?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jan 2022 08:50:38 GMT</pubDate>
    <dc:creator>chrisf</dc:creator>
    <dc:date>2022-01-17T08:50:38Z</dc:date>
    <item>
      <title>LPC546xx power lib</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1400136#M47654</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;we are in the process of migrating several projects to LPC546xx devices. Most of those projects do not use short enum/wchar compile options and are therefore not compatible with the compile settings of the provided power lib for Keil.&lt;/P&gt;&lt;P&gt;Can you please provide us with a version compiled without the short enum/wchar option, or is it possible to circumvent using this library?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 08:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1400136#M47654</guid>
      <dc:creator>chrisf</dc:creator>
      <dc:date>2022-01-17T08:50:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx power lib</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1400948#M47674</link>
      <description>&lt;P&gt;HI&amp;nbsp;chrisf&amp;nbsp;&lt;/P&gt;
&lt;P&gt;LPC55 has&amp;nbsp;keil_lib_power_disable_short_enum_wchar.lib but LPC546xx doesn't have the same. I will escalate it as feature request if necessary. but so far we don't have it.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 12:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1400948#M47674</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-01-18T12:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx power lib</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1401712#M47683</link>
      <description>&lt;P&gt;Hello Jun,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;BR /&gt;We would really appreciate if you could escalate the request and provide us with a library. Changing all connected projects and libraries would probably add weeks or even months to the otherwise relative short task of replacing a BSP. I'd also need to check if all 3rd party libraries are available with this settings.&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 12:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1401712#M47683</guid>
      <dc:creator>chrisf</dc:creator>
      <dc:date>2022-01-19T12:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx power lib</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1402647#M47701</link>
      <description>&lt;P&gt;Hi Chris&lt;/P&gt;
&lt;P&gt;I got it. Thanks.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 13:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-power-lib/m-p/1402647#M47701</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-01-20T13:14:19Z</dc:date>
    </item>
  </channel>
</rss>