<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ?? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392143#M47495</link>
    <description>&lt;P&gt;HI&amp;nbsp;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Maybe I confused the SCTimer clock source and clock input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, SCTimer does not need any external clock input except the system clock. I want to Confirm whether the SCTimer module can work stably if the system clock is greater than 100MHz, such as 180MHz.&lt;/P&gt;&lt;P&gt;The MCU used is lpc54618.&lt;/P&gt;</description>
    <pubDate>Mon, 27 Dec 2021 07:27:36 GMT</pubDate>
    <dc:creator>ZhaiYF</dc:creator>
    <dc:date>2021-12-27T07:27:36Z</dc:date>
    <item>
      <title>LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1391628#M47478</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhaiYF_1-1640313406653.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166164i63F4510ADF52D0D2/image-size/medium?v=v2&amp;amp;px=400" alt="ZhaiYF_1-1640313406653.png" title="ZhaiYF_1-1640313406653.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Question 1、&lt;BR /&gt;In the figure&amp;nbsp; "The maximum frequency for the SCTimer/PWM clock is 100 MHz."&lt;BR /&gt;Is it only applicable for clock after SCTCLKSEL ?&lt;/P&gt;&lt;P&gt;Question 2、&lt;BR /&gt;If set CLKMODE=0 in SCTimer/PWM configuration register。Is there maximum frequency&lt;BR /&gt;limit for system clock ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 03:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1391628#M47478</guid>
      <dc:creator>ZhaiYF</dc:creator>
      <dc:date>2021-12-24T03:09:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392069#M47494</link>
      <description>&lt;P&gt;HI&amp;nbsp;ZhaiYF&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The Maximum freq for SCT is 100Mhz. any input freq. beyond this value is an invalided input and will have un-guaranteed behavior. also , the 100Mhz limit is mainly com from pad limitation. not the SCT module itself&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 05:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392069#M47494</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-12-27T05:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392143#M47495</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Maybe I confused the SCTimer clock source and clock input.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, SCTimer does not need any external clock input except the system clock. I want to Confirm whether the SCTimer module can work stably if the system clock is greater than 100MHz, such as 180MHz.&lt;/P&gt;&lt;P&gt;The MCU used is lpc54618.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 07:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392143#M47495</guid>
      <dc:creator>ZhaiYF</dc:creator>
      <dc:date>2021-12-27T07:27:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54xx The maximum frequency for the SCTimer/PWM clock is 100 MHz ??</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392282#M47496</link>
      <description>&lt;P&gt;Hi&amp;nbsp;ZhaiYF&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are two type of input for SCT,&amp;nbsp;the the 100MHz clock limitation is only valid for the clock source inputted from external pads (SCT_IN7), if you use system clock as the SCTimer/PWM clock source, the system clock frequency can be greater than 100MHz.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1640610687604.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166297iFD51D5AA9D11B961/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1640610687604.png" alt="ZhangJennie_0-1640610687604.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_0-1640610687604.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can also see this "Remarks " &amp;nbsp;immediately below "Select a function clock using SCTCLKSEL (Section 7.5.41)."&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_1-1640610889410.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166298iE81D0872489AB2CE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_1-1640610889410.png" alt="ZhangJennie_1-1640610889410.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZhangJennie_1-1640610889410.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 13:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xx-The-maximum-frequency-for-the-SCTimer-PWM-clock-is-100/m-p/1392282#M47496</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-12-27T13:15:22Z</dc:date>
    </item>
  </channel>
</rss>