<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Connect eMMC to the SD/MMC interface</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connect-eMMC-to-the-SD-MMC-interface/m-p/522094#M4730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Fri Aug 15 04:58:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If I disable the DMA the eMMC work fine, any suggestione?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why with the DMA the system doesn't work?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is not a big problem for the moment, I can continue to develop the code without the DMA, but I want understand what is the cause of the disfunction with the DMA.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:37:08 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:37:08Z</dc:date>
    <item>
      <title>Connect eMMC to the SD/MMC interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connect-eMMC-to-the-SD-MMC-interface/m-p/522093#M4729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Wed Aug 13 09:16:40 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question regarding the eMMC, I'm trying to interface with a Micron eMMC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a Micron eMMC, and I tried to use it by using the same code of the Sd/mmc example provided from LpcOpen, but it seems to doesn't work. (Initialization seems to be ok, but mkfs command not work). The same code work right with a SDHC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe I'm doing something wrong...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it wrong to think that the same code that work with an SDHC memory card should work right also with a eMMC??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alessio&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Connect-eMMC-to-the-SD-MMC-interface/m-p/522093#M4729</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: Connect eMMC to the SD/MMC interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connect-eMMC-to-the-SD-MMC-interface/m-p/522094#M4730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by schisanoa on Fri Aug 15 04:58:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If I disable the DMA the eMMC work fine, any suggestione?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why with the DMA the system doesn't work?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is not a big problem for the moment, I can continue to develop the code without the DMA, but I want understand what is the cause of the disfunction with the DMA.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Connect-eMMC-to-the-SD-MMC-interface/m-p/522094#M4730</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:08Z</dc:date>
    </item>
  </channel>
</rss>