<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Help with FlashMagic and LPCXpresso54018 (OM40003)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-with-FlashMagic-and-LPCXpresso54018-OM40003/m-p/1382444#M47280</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193669" target="_self" aria-label="View Profile of mitchkapa"&gt;&lt;SPAN class=""&gt;mitchkapa&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;Flash Magic only support erase/ program internal flash of chip, there is no internal flash with lp54018, so it can't download .hex file.&lt;/P&gt;
&lt;P&gt;You can use blhost+ flashloader, about detail please refer to:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Dec 2021 07:15:51 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2021-12-07T07:15:51Z</dc:date>
    <item>
      <title>Help with FlashMagic and LPCXpresso54018 (OM40003)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-with-FlashMagic-and-LPCXpresso54018-OM40003/m-p/1381488#M47244</link>
      <description>&lt;P&gt;Hello, I am attempting to use FlashMagic to program the LPC54018 on my LPCXpresso54018 dev board because I am trying to evaluate programming solutions for an upcoming custom board.&amp;nbsp; When I boot the board I have SW4 pressed so that ISP0 is low at boot time.&amp;nbsp; Within FlashMagic I am able to perform a successful Read Signature command (or at least it returns a value and does not show an error) but beyond that I cannot get any other tasks to work.&amp;nbsp; When I try to load a .hex file I get the following message "LPC54018 (LPC54000): Operation Failed. Nothing to program. Is the hex file inside the device memory range?".&amp;nbsp; I also get errors that the Flash Erase operation has failed.&lt;/P&gt;&lt;P&gt;In the FlashMagic preferences I have selected Disable DTR, RTS since those signals are not brought out to the UART header on the board.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If anyone has suggestions or past experience with this I'd appreciate any help.&amp;nbsp; Thanks.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 04 Dec 2021 23:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Help-with-FlashMagic-and-LPCXpresso54018-OM40003/m-p/1381488#M47244</guid>
      <dc:creator>mitchkapa</dc:creator>
      <dc:date>2021-12-04T23:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: Help with FlashMagic and LPCXpresso54018 (OM40003)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-with-FlashMagic-and-LPCXpresso54018-OM40003/m-p/1382444#M47280</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193669" target="_self" aria-label="View Profile of mitchkapa"&gt;&lt;SPAN class=""&gt;mitchkapa&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;Flash Magic only support erase/ program internal flash of chip, there is no internal flash with lp54018, so it can't download .hex file.&lt;/P&gt;
&lt;P&gt;You can use blhost+ flashloader, about detail please refer to:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 07:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Help-with-FlashMagic-and-LPCXpresso54018-OM40003/m-p/1382444#M47280</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-12-07T07:15:51Z</dc:date>
    </item>
  </channel>
</rss>