<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381784#M47262</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;Hi, I drew the block diagram. Since I use a PCB board the connections don't change when I use cp2102 only I take power from my computer's USB port when I connect cp2102 to my computer, but when I connect HC05 I take power from the PCB. So RX, TX connections are the same in both cases.&lt;/P&gt;</description>
    <pubDate>Mon, 06 Dec 2021 09:43:26 GMT</pubDate>
    <dc:creator>Alex_2221</dc:creator>
    <dc:date>2021-12-06T09:43:26Z</dc:date>
    <item>
      <title>LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381517#M47251</link>
      <description>&lt;P&gt;Hello everyone, I'm trying to read temperature and store and send back the data I send. I can do that without any problem using&amp;nbsp;cp2102 USB to TTL module, however when I replace cp2102 module with HC05 bluetooh module when I enter the data instead of the data (two digit number) I enter, I recieve a very long and irrelevant number like 65121. I attached my code.&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Sun, 05 Dec 2021 18:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381517#M47251</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-05T18:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381518#M47252</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;Last time I used your code in this project and it worked perfectly, but now I need to replace cp2102 USB to TTL&amp;nbsp; with HC05 bluetooth module and it doesn't work. What could be the problem?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 05 Dec 2021 18:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381518#M47252</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-05T18:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381672#M47259</link>
      <description>&lt;P&gt;Hi, Alex,&lt;/P&gt;
&lt;P&gt;Can you draw a block diagram so that we can know the connection ? for example, where is the LPC1768, where is the HC05.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 05:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381672#M47259</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-12-06T05:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381784#M47262</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;Hi, I drew the block diagram. Since I use a PCB board the connections don't change when I use cp2102 only I take power from my computer's USB port when I connect cp2102 to my computer, but when I connect HC05 I take power from the PCB. So RX, TX connections are the same in both cases.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 09:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381784#M47262</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-06T09:43:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381858#M47264</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that you have to connect the ground of HC08 to the ground of&amp;nbsp; LPC1768, so that they have the same ground plane.&lt;/P&gt;
&lt;P&gt;Pls check if the two ground are connected together&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 09:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381858#M47264</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-12-06T09:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381876#M47265</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;The ground of the HC05 is connected to the ground of the LPC1768. Plus, I'm able to recieve the temperature from the HC05, but when I enter the data it echos back that large number.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 10:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1381876#M47265</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-06T10:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1382855#M47294</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;This time I used my debugger and realized that the data is properly saving in the variables in debug mode, and only when I want to echo them back using UART_Send when the program is running I recieve a wrong number. My goal was to only save the data and not necessarily echo it. I just wanted to see if I was able to save the data. That's strange though. Anyways, thank you very much for your help. I really appreciate it.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 20:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1382855#M47294</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-07T20:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1383167#M47301</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that the USART_RX pin of LPC17xx is 5V tolerant, the pin can receive 5V logic. But the LPC17xx is 3.3V logic, so the UASRT_TX pin logic voltage of LPC17xx is 3.3V.&lt;/P&gt;
&lt;P&gt;What is your problem now? can you give a clear description?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 06:43:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1383167#M47301</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-12-08T06:43:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 UART works with cp2102 USB to TTL module, but doesn't work with HC05</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1383204#M47303</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp;So as I said. My problem was the fact that I could send data and save it in a variable using cp2102, and I was able to echo it back to see if I managed to save it, however when I replaced cp2102 USB to TTL module with HC05 I realized that I can't echo back the data properly, but when I used my debugger I realized that the data can be properly saved like when I was using cp2102. Only when I run the program I can't echo it back properly. That's strange that I can't echo the data back when I have HC05 instead of cp2102, although it's not necessary to echo back the data. I just wanted to save the data I enter via bluetooth in a variable and it seems like I'm able to do this according to the debugger. So I guess my problem is solved already. Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 07:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-UART-works-with-cp2102-USB-to-TTL-module-but-doesn-t/m-p/1383204#M47303</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-12-08T07:23:54Z</dc:date>
    </item>
  </channel>
</rss>