<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S16 - RAM backup in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381623#M47256</link>
    <description>&lt;P&gt;You are welcome.&lt;/P&gt;</description>
    <pubDate>Mon, 06 Dec 2021 03:34:33 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-12-06T03:34:33Z</dc:date>
    <item>
      <title>LPC55S16 - RAM backup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1380939#M47219</link>
      <description>&lt;P&gt;Is there a way to keep the RAM or some portion of it alive with a backup battery on the LPC55xx micro?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 03:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1380939#M47219</guid>
      <dc:creator>istvanmate</dc:creator>
      <dc:date>2021-12-03T03:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 - RAM backup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381315#M47238</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Power Domain “Always On” includes PMC(Power management controller) and RTC.&lt;/P&gt;
&lt;P&gt;This domain always has power as long as sufficient voltage is available on VBAT ([1.8 V –3.6 V]), that is external battery.&lt;/P&gt;
&lt;P&gt;See below pic. "Always On " domain is in red. While RAM is not controlled by "Always On " domain. So we can't keep RAM with VBAT only.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZhangJennie_0-1638542741826.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164041i5A4A32761E03CF3B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZhangJennie_0-1638542741826.png" alt="ZhangJennie_0-1638542741826.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 14:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381315#M47238</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-12-03T14:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 - RAM backup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381443#M47240</link>
      <description>&lt;P&gt;Thanks for the quick reply.&lt;/P&gt;&lt;P&gt;It is what it is. I'll have to use external means to keep data alive between power cycles.&lt;/P&gt;</description>
      <pubDate>Sat, 04 Dec 2021 00:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381443#M47240</guid>
      <dc:creator>istvanmate</dc:creator>
      <dc:date>2021-12-04T00:20:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 - RAM backup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381623#M47256</link>
      <description>&lt;P&gt;You are welcome.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 03:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-RAM-backup/m-p/1381623#M47256</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-12-06T03:34:33Z</dc:date>
    </item>
  </channel>
</rss>