<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LCP55S69 with 7inch touch screen? (feasible..?) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S69-with-7inch-touch-screen-feasible/m-p/1381522#M47253</link>
    <description>&lt;P&gt;Hey&lt;BR /&gt;&lt;BR /&gt;I'm planning to use the LCP55S69 for an LVGL project. I know there is an example project and i believe that drives a 2.8" screen.&lt;BR /&gt;I'm going to connect to an FT813 controller with 7in 800x480pixel display. As the controller is capable of driving this display and the requirements for PI communication to the controller are possible with the LCP board, this seems to me as a feasible option.&lt;BR /&gt;However, is there anything I'm overlooking? Will this evaluation board be capable of this project considering the FT813 is capable of driving the screen?&lt;BR /&gt;&lt;BR /&gt;Sorry for the somewhat specific yet vague question but would love a pointer if anyone has experience with this board.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Lexi&lt;/P&gt;</description>
    <pubDate>Sun, 05 Dec 2021 22:37:00 GMT</pubDate>
    <dc:creator>BabyBorisova</dc:creator>
    <dc:date>2021-12-05T22:37:00Z</dc:date>
    <item>
      <title>LCP55S69 with 7inch touch screen? (feasible..?)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S69-with-7inch-touch-screen-feasible/m-p/1381522#M47253</link>
      <description>&lt;P&gt;Hey&lt;BR /&gt;&lt;BR /&gt;I'm planning to use the LCP55S69 for an LVGL project. I know there is an example project and i believe that drives a 2.8" screen.&lt;BR /&gt;I'm going to connect to an FT813 controller with 7in 800x480pixel display. As the controller is capable of driving this display and the requirements for PI communication to the controller are possible with the LCP board, this seems to me as a feasible option.&lt;BR /&gt;However, is there anything I'm overlooking? Will this evaluation board be capable of this project considering the FT813 is capable of driving the screen?&lt;BR /&gt;&lt;BR /&gt;Sorry for the somewhat specific yet vague question but would love a pointer if anyone has experience with this board.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Lexi&lt;/P&gt;</description>
      <pubDate>Sun, 05 Dec 2021 22:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S69-with-7inch-touch-screen-feasible/m-p/1381522#M47253</guid>
      <dc:creator>BabyBorisova</dc:creator>
      <dc:date>2021-12-05T22:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: LCP55S69 with 7inch touch screen? (feasible..?)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S69-with-7inch-touch-screen-feasible/m-p/1381674#M47260</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We&amp;nbsp; have littlevgl_examples under MCUXpresso SDK for&amp;nbsp; Adafruit TFT LCD shield w/Cap Touch V2.3, SPI display. Besides, we don't have other existing demo.&amp;nbsp; User needs to refer our demo to adjust code by self.&lt;/P&gt;
&lt;P&gt;There are different versions of Adafruit 2.8" TFT LCD shields. The shields marked v2.0 works directly with this project. For the other shields, please solder the center pin of IOREF pads to the 3.3V pad, and solder the pads 11, 12, and 13.&lt;BR /&gt;See the link for details:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LCD-for-SDK-graphics/ba-p/1131104" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LCD-for-SDK-graphics/ba-p/1131104&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Besides, NXP has partnered with SEGGER Microcontroller to offer high performance embedded graphics libraries in binary form for free commercial use. FYI.&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 06:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCP55S69-with-7inch-touch-screen-feasible/m-p/1381674#M47260</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-12-06T06:50:42Z</dc:date>
    </item>
  </channel>
</rss>