<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Fully Differential ADC Mode LPC4370 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fully-Differential-ADC-Mode-LPC4370/m-p/1380975#M47221</link>
    <description>&lt;P&gt;Hi NXP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have some questions about using the LPC4370 (Link2 dev board) ADC in fully differential mode. I am wanting to drive the ADC from a fully differential output (ADRF6510 amplifier), but the minimum common mode voltage I can achieve with the amplifier is 1.5V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it true that I need to supply one of the outputs of the amplifier to the ADCHS_NEG pin? And is it also true that this ADCHS_NEG voltage needs to remain within around 0-1V?&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the data sheets it often assumes that you are not supplying anything to this ADCHC_NEG pin and use the nominal 0.5V, which makes sense that you have to swing around that 0.5V ± 0.4V. But it is not clear to me what happens if you use a higher voltage such as 1.5V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It probably won't work, but just want to make sure before implementing a more complicated solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Quinn&lt;/P&gt;</description>
    <pubDate>Fri, 03 Dec 2021 05:13:08 GMT</pubDate>
    <dc:creator>QM</dc:creator>
    <dc:date>2021-12-03T05:13:08Z</dc:date>
    <item>
      <title>Fully Differential ADC Mode LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fully-Differential-ADC-Mode-LPC4370/m-p/1380975#M47221</link>
      <description>&lt;P&gt;Hi NXP,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have some questions about using the LPC4370 (Link2 dev board) ADC in fully differential mode. I am wanting to drive the ADC from a fully differential output (ADRF6510 amplifier), but the minimum common mode voltage I can achieve with the amplifier is 1.5V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it true that I need to supply one of the outputs of the amplifier to the ADCHS_NEG pin? And is it also true that this ADCHS_NEG voltage needs to remain within around 0-1V?&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the data sheets it often assumes that you are not supplying anything to this ADCHC_NEG pin and use the nominal 0.5V, which makes sense that you have to swing around that 0.5V ± 0.4V. But it is not clear to me what happens if you use a higher voltage such as 1.5V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It probably won't work, but just want to make sure before implementing a more complicated solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Quinn&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 05:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Fully-Differential-ADC-Mode-LPC4370/m-p/1380975#M47221</guid>
      <dc:creator>QM</dc:creator>
      <dc:date>2021-12-03T05:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: Fully Differential ADC Mode LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Fully-Differential-ADC-Mode-LPC4370/m-p/1381882#M47266</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the following fig in data sheet of LPC4370, the ADCHS_NEG is 350 mV&amp;lt;Vin_neg&amp;lt;900 mV.&lt;/P&gt;
&lt;P&gt;If the common mode voltage of ADRF6510 differential output is 1.5V at least, I suppose you can not connect the ADRF6510 differential output to ADCHS_NEG directly.&lt;/P&gt;
&lt;P&gt;I suppose you can use AMP to establish a differential to single-ended converter and connect to analog pin of LPC4370&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1638785485558.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164185i7482DF7229DC7D18/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1638785485558.png" alt="xiangjun_rong_1-1638785485558.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_1-1638785485558.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1638785020253.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164182iDA192DCCC6034BF3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1638785020253.png" alt="xiangjun_rong_0-1638785020253.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1638785020253.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 10:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Fully-Differential-ADC-Mode-LPC4370/m-p/1381882#M47266</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-12-06T10:13:34Z</dc:date>
    </item>
  </channel>
</rss>