<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックEthernet IEEE 1588 target time register</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1377592#M47127</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in the LPC540xx user guide (UM11060), page 831, there is the flag TSTRIG&lt;/P&gt;&lt;P&gt;"Enable timestamp interrupt trigger.&lt;BR /&gt;When this bit is set, the timestamp interrupt is generated when the system time&lt;BR /&gt;becomes greater than the value written in the target time register. This bit is reset&lt;BR /&gt;after the timestamp trigger interrupt is generated."&lt;/P&gt;&lt;P&gt;But I can't find the target time register, so I am not sure when the interrupt is going to be triggered.&lt;/P&gt;&lt;P&gt;Is this feature implemented?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 Nov 2021 10:50:33 GMT</pubDate>
    <dc:creator>matteo_vit</dc:creator>
    <dc:date>2021-11-26T10:50:33Z</dc:date>
    <item>
      <title>Ethernet IEEE 1588 target time register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1377592#M47127</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in the LPC540xx user guide (UM11060), page 831, there is the flag TSTRIG&lt;/P&gt;&lt;P&gt;"Enable timestamp interrupt trigger.&lt;BR /&gt;When this bit is set, the timestamp interrupt is generated when the system time&lt;BR /&gt;becomes greater than the value written in the target time register. This bit is reset&lt;BR /&gt;after the timestamp trigger interrupt is generated."&lt;/P&gt;&lt;P&gt;But I can't find the target time register, so I am not sure when the interrupt is going to be triggered.&lt;/P&gt;&lt;P&gt;Is this feature implemented?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 10:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1377592#M47127</guid>
      <dc:creator>matteo_vit</dc:creator>
      <dc:date>2021-11-26T10:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet IEEE 1588 target time register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1378031#M47144</link>
      <description>&lt;P&gt;Hi Matteo&lt;/P&gt;
&lt;P&gt;I sent you message for more information needed.&lt;/P&gt;
&lt;P&gt;Please have a look.&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 29 Nov 2021 07:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1378031#M47144</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-11-29T07:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet IEEE 1588 target time register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1703677#M53836</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;do you have a reply to your question ?&lt;/P&gt;&lt;P&gt;I've got exactly the same (where is the target time register for the TSTRIG) in my lpc54s018, but nothing in the documentation, and nothing in NXP forums&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice will be welcome&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Fri, 11 Aug 2023 17:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1703677#M53836</guid>
      <dc:creator>ppardo</dc:creator>
      <dc:date>2023-08-11T17:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet IEEE 1588 target time register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1704109#M53842</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I need this reply too.&lt;/P&gt;&lt;P&gt;In documentation, for TSIS, where's the target time registers ?&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;Timestamp interrupt status.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;This bit is set when any of the following conditions is true:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;The system time value equals or exceeds the value specified in the target time&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;high and low registers.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;There is an overflow in the seconds register.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;This bit is cleared on reading the byte 0 of the timestamp status register&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;(Table 798).&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;When default timestamping is enabled, this bit when set indicates that the system&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;time value equals or exceeds the value specified in &lt;STRONG&gt;the target time registers&lt;/STRONG&gt;. In this&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;mode, this bit is cleared after the completion of the read of this interrupt status&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;register[9]. In all other modes, this bit is reserved.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 07:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-IEEE-1588-target-time-register/m-p/1704109#M53842</guid>
      <dc:creator>ppardo</dc:creator>
      <dc:date>2023-08-14T07:10:11Z</dc:date>
    </item>
  </channel>
</rss>