<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: About (LPC54018 OM40003) USB Power</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC54018-OM40003-USB-Power/m-p/1375292#M47080</link>
    <description>&lt;P&gt;Yes, you can use USB power this way.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Nov 2021 02:21:16 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-11-23T02:21:16Z</dc:date>
    <item>
      <title>About (LPC54018 OM40003) USB Power</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC54018-OM40003-USB-Power/m-p/1375148#M47078</link>
      <description>&lt;P&gt;Heyy,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using an OM40003 board and &lt;STRONG&gt;I need to know if I can use the board with the two USB, shown in the file, connected and powered on at the same time.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need both at the same time because in full operation I use a source as the main power(without using computer usb for Debug), and at another time I need to use a source and the computer for debug (passing 5 volts also from the computer's USB).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Rodrigo Almeida.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Nov 2021 17:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC54018-OM40003-USB-Power/m-p/1375148#M47078</guid>
      <dc:creator>RodrigoEngComp</dc:creator>
      <dc:date>2021-11-22T17:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: About (LPC54018 OM40003) USB Power</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC54018-OM40003-USB-Power/m-p/1375292#M47080</link>
      <description>&lt;P&gt;Yes, you can use USB power this way.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 02:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC54018-OM40003-USB-Power/m-p/1375292#M47080</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-11-23T02:21:16Z</dc:date>
    </item>
  </channel>
</rss>