<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Max ext clock frequency LPC550x</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1369821#M46979</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that there is discrepancy for the required crystal clock frequency spec and external clock frequency spec in data sheet Rev1.2 of LPC550x, I have submitted a ticket to AE team so that they can confirm.&lt;/P&gt;
&lt;P&gt;I will give you a feedback after I get response.&lt;/P&gt;
&lt;P&gt;sorry to the inconvenience.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 11 Nov 2021 09:03:44 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-11-11T09:03:44Z</dc:date>
    <item>
      <title>Max ext clock frequency LPC550x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1369703#M46976</link>
      <description>&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;I'm wondering what the max. frequency of external clock in bypass mode on the LPC550x is.&lt;/P&gt;&lt;P&gt;From LPC55S0x/LPC550x product datasheet Rev. 1.2 - 6. August 2021:&lt;/P&gt;&lt;P&gt;Page 4 reads: "Crystal oscillator with an operating frequency of 12 MHz to 32 MHz. Option for&lt;BR /&gt;external clock input (bypass mode) for clock frequencies of &lt;STRONG&gt;up to 25 MHz&lt;/STRONG&gt;."&lt;/P&gt;&lt;P&gt;Page 98 reads: "In bypass mode, an external clock (maximum frequency of &lt;STRONG&gt;up to 24 MHz&lt;/STRONG&gt;) can also be&lt;BR /&gt;connected to XTAL32M_P if XTAL32M_N is left open."&lt;/P&gt;&lt;P&gt;So that does not seem to be consistent. Was the spec. extended from 24 MHz to 25 MHz, and not all references updated?&lt;/P&gt;&lt;P&gt;Is it allowed to run LPC550x with 25 MHz external clock?&lt;/P&gt;&lt;P&gt;Many thanks in advance,&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 06:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1369703#M46976</guid>
      <dc:creator>ThomasO</dc:creator>
      <dc:date>2021-11-11T06:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Max ext clock frequency LPC550x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1369821#M46979</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see that there is discrepancy for the required crystal clock frequency spec and external clock frequency spec in data sheet Rev1.2 of LPC550x, I have submitted a ticket to AE team so that they can confirm.&lt;/P&gt;
&lt;P&gt;I will give you a feedback after I get response.&lt;/P&gt;
&lt;P&gt;sorry to the inconvenience.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 09:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1369821#M46979</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-11-11T09:03:44Z</dc:date>
    </item>
    <item>
      <title>Re: Max ext clock frequency LPC550x</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1372352#M47024</link>
      <description>&lt;P&gt;Hi, Thomas,&lt;/P&gt;
&lt;P&gt;For crystal oscillator spec range, it is 12 MHz to 32 MHz. 1 MHz to 25 MHz is not correct.&lt;/P&gt;
&lt;P&gt;For usage of bypass mode, maximum is indeed 24 Mhz since that is it what tested in bypass mode.&lt;/P&gt;
&lt;P&gt;The bypass mode&amp;nbsp; is not true bypass anything, the clock signal will be processed by Crystal oscillator.&lt;/P&gt;
&lt;P&gt;so you should follow up the spec in datasheet as following for the external clock voltage: &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1637119458012.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/162343iFD7B957007FDCF9D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1637119458012.png" alt="xiangjun_rong_0-1637119458012.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 03:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-ext-clock-frequency-LPC550x/m-p/1372352#M47024</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-11-17T03:26:58Z</dc:date>
    </item>
  </channel>
</rss>