<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSD/MMC Questions</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-MMC-Questions/m-p/522059#M4695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bunrockter on Sat Aug 04 13:43:37 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I recently got the Hitex board and I am trying to get the SD peripheral up and running. I have chose not to use the driver the comes with the 4350 because I am using a state based design, and I want to tightly integrate it with a state machine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have looked at the code, and set up my initialization accordingly. I get and interrupt for card presence, but I am unable to get a Remote timeout or command done interrupt to fire. I am trying to send the idle command to the card (which I know doesn't respond) but I would expect to get a command done interrupt &amp;amp; I don't.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is setting up the args register, and setting the START_CMD bit in the CMD register all I have to do to send a command?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:37:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:37:45Z</dc:date>
    <item>
      <title>SD/MMC Questions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-MMC-Questions/m-p/522059#M4695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bunrockter on Sat Aug 04 13:43:37 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I recently got the Hitex board and I am trying to get the SD peripheral up and running. I have chose not to use the driver the comes with the 4350 because I am using a state based design, and I want to tightly integrate it with a state machine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have looked at the code, and set up my initialization accordingly. I get and interrupt for card presence, but I am unable to get a Remote timeout or command done interrupt to fire. I am trying to send the idle command to the card (which I know doesn't respond) but I would expect to get a command done interrupt &amp;amp; I don't.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is setting up the args register, and setting the START_CMD bit in the CMD register all I have to do to send a command?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-MMC-Questions/m-p/522059#M4695</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: SD/MMC Questions</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SD-MMC-Questions/m-p/522060#M4696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mirfan on Mon Sep 24 05:43:03 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi bunrockter,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the START_CMD bit getting cleared after you set the CMD register? CIU clears this bit once it accepts the command.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SD-MMC-Questions/m-p/522060#M4696</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:46Z</dc:date>
    </item>
  </channel>
</rss>