<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S69-EVK Simultaneous USB Host and Device in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Simultaneous-USB-Host-and-Device/m-p/1368051#M46944</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about this dev board and this microcontroller. What I would like to do, is have both a USB device and a USB host on one microcontroller, acting as a "proxy" for the USB device connected to the board.&lt;/P&gt;&lt;P&gt;The user manual mentions that either port can be configured as a host at once in section 6.1, but nothing on using one as a host and one as a device. Is this a possible thing to do with this platform? If not, where else should I look within NXP microcontrollers?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Mon, 08 Nov 2021 22:10:17 GMT</pubDate>
    <dc:creator>ja2022</dc:creator>
    <dc:date>2021-11-08T22:10:17Z</dc:date>
    <item>
      <title>LPC55S69-EVK Simultaneous USB Host and Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Simultaneous-USB-Host-and-Device/m-p/1368051#M46944</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about this dev board and this microcontroller. What I would like to do, is have both a USB device and a USB host on one microcontroller, acting as a "proxy" for the USB device connected to the board.&lt;/P&gt;&lt;P&gt;The user manual mentions that either port can be configured as a host at once in section 6.1, but nothing on using one as a host and one as a device. Is this a possible thing to do with this platform? If not, where else should I look within NXP microcontrollers?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 22:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Simultaneous-USB-Host-and-Device/m-p/1368051#M46944</guid>
      <dc:creator>ja2022</dc:creator>
      <dc:date>2021-11-08T22:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69-EVK Simultaneous USB Host and Device</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Simultaneous-USB-Host-and-Device/m-p/1368146#M46947</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;Yes you can&amp;nbsp;&lt;SPAN&gt;have both a USB device and a USB host on one microcontroller.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I suggest you setting different&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;task priority&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;on each task when created. You could take keyboard2mouse sdk example as reference.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 02:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-EVK-Simultaneous-USB-Host-and-Device/m-p/1368146#M46947</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-11-09T02:54:40Z</dc:date>
    </item>
  </channel>
</rss>