<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックExternal Trigger to HSADC using SGPIO10</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1363328#M46900</link>
    <description>&lt;P&gt;Kindly suggest a way to trigger HSADC of LPC 4370 using SGPIO10. If possible then please send the snippet of the code as well. &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129105"&gt;@ravithakur&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 28 Oct 2021 13:26:09 GMT</pubDate>
    <dc:creator>shivam0078</dc:creator>
    <dc:date>2021-10-28T13:26:09Z</dc:date>
    <item>
      <title>External Trigger to HSADC using SGPIO10</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1363328#M46900</link>
      <description>&lt;P&gt;Kindly suggest a way to trigger HSADC of LPC 4370 using SGPIO10. If possible then please send the snippet of the code as well. &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/129105"&gt;@ravithakur&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 13:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1363328#M46900</guid>
      <dc:creator>shivam0078</dc:creator>
      <dc:date>2021-10-28T13:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: External Trigger to HSADC using SGPIO10</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1363652#M46904</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;we do not know what logic of SGPIO you would like to implement, anyway, I think an11275.zip is helpful for your understanding SGPIO module, pls refer to it.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN11275.zip" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN11275.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 29 Oct 2021 05:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1363652#M46904</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-10-29T05:14:00Z</dc:date>
    </item>
    <item>
      <title>Re: External Trigger to HSADC using SGPIO10</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1385458#M47364</link>
      <description>&lt;P&gt;Thanks for your reply. I want a trigger pin using which I can trigger the hsadc externally in lpc link 2 board. From the datasheet I have found that I can trigger the hsadc using SGPIO10. I have configured the sgpio10 to the P1_3 pin of LPC4370 controller. Then I have connected the SGPIO10 as a trigger to HSADC using GIMA. Please suggest me a way to trigger HSADC externally.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 08:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/External-Trigger-to-HSADC-using-SGPIO10/m-p/1385458#M47364</guid>
      <dc:creator>shivam0078</dc:creator>
      <dc:date>2021-12-13T08:10:52Z</dc:date>
    </item>
  </channel>
</rss>