<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SYSAHBCLKCTRL in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1358708#M46833</link>
    <description>&lt;P&gt;Found it - it's&amp;nbsp;&lt;SPAN&gt;AHBCLKCTRL - I was looking for something that started with SYS.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Oct 2021 14:04:50 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2021-10-20T14:04:50Z</dc:date>
    <item>
      <title>SYSAHBCLKCTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1357927#M46828</link>
      <description>&lt;P&gt;I'm just migrating my code from LPC1517 to LPC5502 (because that's all I can get). LPC8, LPC11, LPC13 and LPC15 all require bits to be set in SYSAHBCLKCTRL in order to enable any particular peripheral.&lt;/P&gt;&lt;P&gt;The LPC5502 appears not to have a SYSAHBCLKCTRL register - what takes it place?&lt;/P&gt;&lt;P&gt;It is only mentioned in the manual in Fig.86 "Watchdog timer clocking".&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 13:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1357927#M46828</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-10-19T13:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: SYSAHBCLKCTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1358708#M46833</link>
      <description>&lt;P&gt;Found it - it's&amp;nbsp;&lt;SPAN&gt;AHBCLKCTRL - I was looking for something that started with SYS.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 14:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1358708#M46833</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-10-20T14:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: SYSAHBCLKCTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1362197#M46891</link>
      <description>&lt;P&gt;But that means that the reference in the watchdog timer section must be wrong?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 07:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1362197#M46891</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-10-27T07:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: SYSAHBCLKCTRL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1363981#M46906</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132886"&gt;@ianbenton&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Chapter 29 in the User Manual, show the basic configuration for the watchdog the is the following:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Configure WDTCLKDIV register. See Table 103. Release the reset, disable HALT bit&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;and program DIV[5:0].&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Enable the register interface (WWDT bus clock): set the WWDT bit in the&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;AHBCLKCTRL0 register, see Table 55.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;For waking up from a WWDT interrupt, enable the watchdog interrupt for wake-up using low power API.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The AHBCLKCTRL0 bit for the WWDT has to be enable, please give me more information&amp;nbsp; why this could be wrong.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Oct 2021 14:38:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SYSAHBCLKCTRL/m-p/1363981#M46906</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2021-10-29T14:38:36Z</dc:date>
    </item>
  </channel>
</rss>