<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LCD Controller configuration</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-Controller-configuration/m-p/522043#M4679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvey_13 on Wed Jan 30 04:05:22 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm testing an EA LPC1788 OEM Board with it sbase board and a KYOCERA 320x240 TFT Display 24 bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I made different tests which works fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I plan to use µEZ, so I adapt the version 1.11 for my lcd with success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I want ot use the version 2.03 I made the same modification on it but it doesn't works :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; On the external memory, the address 0xa0000000 and 0xa0000004 are displayed on the same display bit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Normally each 4 bytes group match a lcd bit, but in this case each bit is controlled by a 8 bytes memory ......&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked the LPC_LCD register and they are correct .&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What other register may make this behaviuor ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:37:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:37:28Z</dc:date>
    <item>
      <title>LCD Controller configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-Controller-configuration/m-p/522043#M4679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvey_13 on Wed Jan 30 04:05:22 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm testing an EA LPC1788 OEM Board with it sbase board and a KYOCERA 320x240 TFT Display 24 bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I made different tests which works fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I plan to use µEZ, so I adapt the version 1.11 for my lcd with success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I want ot use the version 2.03 I made the same modification on it but it doesn't works :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; On the external memory, the address 0xa0000000 and 0xa0000004 are displayed on the same display bit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Normally each 4 bytes group match a lcd bit, but in this case each bit is controlled by a 8 bytes memory ......&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked the LPC_LCD register and they are correct .&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What other register may make this behaviuor ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-Controller-configuration/m-p/522043#M4679</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Controller configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-Controller-configuration/m-p/522044#M4680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Harvey_13 on Wed Jan 30 07:42:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm sorry the problem was not coming from the LPC Controller. When I write directly in memory everything works correctly...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In fact it comes from the µEZ lib which does not compile as expected and write only 16bit date instead of 32bits.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;**Post Cancelled**&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LCD-Controller-configuration/m-p/522044#M4680</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:30Z</dc:date>
    </item>
  </channel>
</rss>