<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1788 memory  allocation Problem  with FreeRTOS+TCP(Ethernet )</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-memory-allocation-Problem-with-FreeRTOS-TCP-Ethernet/m-p/1352588#M46670</link>
    <description>&lt;P&gt;We are using LPC1788 OEM Board REV E.of Embedded Artists.&lt;BR /&gt;We are using MCUXpresso IDE V11.3.0 and FreeRTOS Lwip stack.&lt;/P&gt;&lt;P&gt;When we use RAM_32 for Heap and Stack Placement our Application works fine,&amp;nbsp;but we need more RAM space hence we changed RAM_32 to RAM_64 .&lt;/P&gt;&lt;P&gt;However with RAM_64 application is not working properly.(Ethernet communication not working).&lt;/P&gt;</description>
    <pubDate>Fri, 08 Oct 2021 09:46:45 GMT</pubDate>
    <dc:creator>pratap1</dc:creator>
    <dc:date>2021-10-08T09:46:45Z</dc:date>
    <item>
      <title>LPC1788 memory  allocation Problem  with FreeRTOS+TCP(Ethernet )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-memory-allocation-Problem-with-FreeRTOS-TCP-Ethernet/m-p/1352588#M46670</link>
      <description>&lt;P&gt;We are using LPC1788 OEM Board REV E.of Embedded Artists.&lt;BR /&gt;We are using MCUXpresso IDE V11.3.0 and FreeRTOS Lwip stack.&lt;/P&gt;&lt;P&gt;When we use RAM_32 for Heap and Stack Placement our Application works fine,&amp;nbsp;but we need more RAM space hence we changed RAM_32 to RAM_64 .&lt;/P&gt;&lt;P&gt;However with RAM_64 application is not working properly.(Ethernet communication not working).&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 09:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-memory-allocation-Problem-with-FreeRTOS-TCP-Ethernet/m-p/1352588#M46670</guid>
      <dc:creator>pratap1</dc:creator>
      <dc:date>2021-10-08T09:46:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 memory  allocation Problem  with FreeRTOS+TCP(Ethernet )</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-memory-allocation-Problem-with-FreeRTOS-TCP-Ethernet/m-p/1353054#M46691</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you post your code so that we can have a review?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;</description>
      <pubDate>Sat, 09 Oct 2021 08:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-memory-allocation-Problem-with-FreeRTOS-TCP-Ethernet/m-p/1353054#M46691</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-10-09T08:21:51Z</dc:date>
    </item>
  </channel>
</rss>