<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1788 Etherate based Project  suddenly stops working  After Random Time intervals.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350912#M46640</link>
    <description>&lt;P&gt;There is still not much to work on for somebody not sitting in front of this board.&lt;/P&gt;&lt;P&gt;Run your application in the debugger, and check where it ends up when communication stops. I still think it is the hardfault handler. If so, check the SCB registers to get more information about the fault cause.&lt;/P&gt;&lt;P&gt;Otherwise, you can instrument your code (add log/output code to observe it without debugger).&lt;/P&gt;&lt;P&gt;Or use the additional trace channel of the debugger (if you spent the extra money for a professional debug pod and tool chain that supports it).&lt;/P&gt;</description>
    <pubDate>Wed, 06 Oct 2021 06:20:06 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2021-10-06T06:20:06Z</dc:date>
    <item>
      <title>LPC1788 Etherate based Project  suddenly stops working  After Random Time intervals.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350605#M46632</link>
      <description>&lt;P&gt;LPC1788 Etherate based Project suddenly stops working (HANGED) After Random Time intervals.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 12:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350605#M46632</guid>
      <dc:creator>pratap1</dc:creator>
      <dc:date>2021-10-05T12:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 Etherate based Project  suddenly stops working  After Random Time intervals.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350613#M46633</link>
      <description>&lt;P&gt;My crystal ball says your power supply fails periodically ...&lt;/P&gt;&lt;P&gt;But honestly, you need to provide more and specific information to receive help.&lt;/P&gt;&lt;P&gt;I suspect a stack overflow, and a subsequent hardfault.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 12:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350613#M46633</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-10-05T12:47:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 Etherate based Project  suddenly stops working  After Random Time intervals.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350909#M46638</link>
      <description>&lt;P&gt;We are using LPC1788 OEM Board REV E.of Embedded Artists.&lt;/P&gt;&lt;P&gt;We are using MCUXpresso IDE V11.3.0 and FreeRTOS Lwip stack.&lt;/P&gt;&lt;P&gt;This Board uses a socket communication to communicate with other board at 1ms time interval. Randomly after few hours the LPC1788 Board stops working. The socket communication stops and the continuously Blinking test LED also Stops Blinking.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 06:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350909#M46638</guid>
      <dc:creator>pratap1</dc:creator>
      <dc:date>2021-10-06T06:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 Etherate based Project  suddenly stops working  After Random Time intervals.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350912#M46640</link>
      <description>&lt;P&gt;There is still not much to work on for somebody not sitting in front of this board.&lt;/P&gt;&lt;P&gt;Run your application in the debugger, and check where it ends up when communication stops. I still think it is the hardfault handler. If so, check the SCB registers to get more information about the fault cause.&lt;/P&gt;&lt;P&gt;Otherwise, you can instrument your code (add log/output code to observe it without debugger).&lt;/P&gt;&lt;P&gt;Or use the additional trace channel of the debugger (if you spent the extra money for a professional debug pod and tool chain that supports it).&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 06:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Etherate-based-Project-suddenly-stops-working-After/m-p/1350912#M46640</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-10-06T06:20:06Z</dc:date>
    </item>
  </channel>
</rss>