<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54113 no acces via SWD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-no-acces-via-SWD/m-p/1346327#M46578</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we use the LPC54113 within our custom Board.&lt;/P&gt;&lt;P&gt;But we can't acces the µC via SWD.&lt;/P&gt;&lt;P&gt;We strip down the PCB up to only the µC and the capacitor.&lt;/P&gt;&lt;P&gt;So there are no other connections, beside the SWD Signals.&lt;/P&gt;&lt;P&gt;Via the Segger j-link we can connect to the µC, but any further acces is not possible.&lt;/P&gt;&lt;P&gt;We teted 4 Boards and 3 different j-links.&lt;/P&gt;&lt;P&gt;The Voltage is 3.3V and there is no ripple.&lt;/P&gt;&lt;P&gt;Here you can see the Log from the j-link:&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;- Connecting via USB to probe/ programmer device 0&lt;BR /&gt;- Probe/ Programmer firmware: J-Link EDU Mini V1 compiled Jun 24 2021 14:29:39&lt;BR /&gt;- Device "LPC54113J256_M4" selected.&lt;BR /&gt;- Target interface speed: 100 kHz (Fixed)&lt;BR /&gt;- VTarget = 3.291V&lt;BR /&gt;- Found SW-DP with ID 0x2BA01477&lt;BR /&gt;- DPIDR: 0x2BA01477&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[1]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x24770011)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Core found&lt;BR /&gt;- AP[0]: AHB-AP ROM base: 0xE00FF000&lt;BR /&gt;- CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)&lt;BR /&gt;- Found Cortex-M4 r0p1, Little endian.&lt;BR /&gt;- FPUnit: 6 code (BP) slots and 2 literal slots&lt;BR /&gt;- CoreSight components:&lt;BR /&gt;- ROMTbl[0] @ E00FF000&lt;BR /&gt;- ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt;- ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT&lt;BR /&gt;- ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB&lt;BR /&gt;- ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM&lt;BR /&gt;- ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU&lt;BR /&gt;- Executing init sequence ...&lt;BR /&gt;- Initialized successfully&lt;BR /&gt;- Target interface speed: 100 kHz (Fixed)&lt;BR /&gt;- CPU clock frequency: 5981 kHz (Auto detected)&lt;BR /&gt;- Found 1 JTAG device. Core ID: 0x2BA01477 (None)&lt;BR /&gt;- Connected successfully&lt;BR /&gt;Blank checking target ...&lt;BR /&gt;- 8 of 8 sectors selected, 1 range, 0x0 - 0x3FFFF&lt;BR /&gt;- Start of preparing flash programming&lt;BR /&gt;- ERROR: Failed to download RAMCode.&lt;BR /&gt;- ERROR: Failed to prepare for programming.&lt;BR /&gt;Failed to download RAMCode!&lt;BR /&gt;- End of preparing flash programming&lt;BR /&gt;- Start of restoring&lt;BR /&gt;- End of restoring&lt;BR /&gt;- ERROR: Failed to check blank target&lt;BR /&gt;Disconnecting ...&lt;BR /&gt;- Disconnected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any hints, what is going wrong?&lt;/P&gt;&lt;P&gt;Is there any protection preprogrammed ?&lt;/P&gt;&lt;P&gt;What else should i check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks Andreas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 26 Sep 2021 15:40:27 GMT</pubDate>
    <dc:creator>andreasruetten</dc:creator>
    <dc:date>2021-09-26T15:40:27Z</dc:date>
    <item>
      <title>LPC54113 no acces via SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-no-acces-via-SWD/m-p/1346327#M46578</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we use the LPC54113 within our custom Board.&lt;/P&gt;&lt;P&gt;But we can't acces the µC via SWD.&lt;/P&gt;&lt;P&gt;We strip down the PCB up to only the µC and the capacitor.&lt;/P&gt;&lt;P&gt;So there are no other connections, beside the SWD Signals.&lt;/P&gt;&lt;P&gt;Via the Segger j-link we can connect to the µC, but any further acces is not possible.&lt;/P&gt;&lt;P&gt;We teted 4 Boards and 3 different j-links.&lt;/P&gt;&lt;P&gt;The Voltage is 3.3V and there is no ripple.&lt;/P&gt;&lt;P&gt;Here you can see the Log from the j-link:&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;- Connecting via USB to probe/ programmer device 0&lt;BR /&gt;- Probe/ Programmer firmware: J-Link EDU Mini V1 compiled Jun 24 2021 14:29:39&lt;BR /&gt;- Device "LPC54113J256_M4" selected.&lt;BR /&gt;- Target interface speed: 100 kHz (Fixed)&lt;BR /&gt;- VTarget = 3.291V&lt;BR /&gt;- Found SW-DP with ID 0x2BA01477&lt;BR /&gt;- DPIDR: 0x2BA01477&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[1]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x24770011)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Core found&lt;BR /&gt;- AP[0]: AHB-AP ROM base: 0xE00FF000&lt;BR /&gt;- CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)&lt;BR /&gt;- Found Cortex-M4 r0p1, Little endian.&lt;BR /&gt;- FPUnit: 6 code (BP) slots and 2 literal slots&lt;BR /&gt;- CoreSight components:&lt;BR /&gt;- ROMTbl[0] @ E00FF000&lt;BR /&gt;- ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7&lt;BR /&gt;- ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT&lt;BR /&gt;- ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB&lt;BR /&gt;- ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM&lt;BR /&gt;- ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU&lt;BR /&gt;- Executing init sequence ...&lt;BR /&gt;- Initialized successfully&lt;BR /&gt;- Target interface speed: 100 kHz (Fixed)&lt;BR /&gt;- CPU clock frequency: 5981 kHz (Auto detected)&lt;BR /&gt;- Found 1 JTAG device. Core ID: 0x2BA01477 (None)&lt;BR /&gt;- Connected successfully&lt;BR /&gt;Blank checking target ...&lt;BR /&gt;- 8 of 8 sectors selected, 1 range, 0x0 - 0x3FFFF&lt;BR /&gt;- Start of preparing flash programming&lt;BR /&gt;- ERROR: Failed to download RAMCode.&lt;BR /&gt;- ERROR: Failed to prepare for programming.&lt;BR /&gt;Failed to download RAMCode!&lt;BR /&gt;- End of preparing flash programming&lt;BR /&gt;- Start of restoring&lt;BR /&gt;- End of restoring&lt;BR /&gt;- ERROR: Failed to check blank target&lt;BR /&gt;Disconnecting ...&lt;BR /&gt;- Disconnected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any hints, what is going wrong?&lt;/P&gt;&lt;P&gt;Is there any protection preprogrammed ?&lt;/P&gt;&lt;P&gt;What else should i check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks Andreas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 26 Sep 2021 15:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-no-acces-via-SWD/m-p/1346327#M46578</guid>
      <dc:creator>andreasruetten</dc:creator>
      <dc:date>2021-09-26T15:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54113 no acces via SWD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-no-acces-via-SWD/m-p/1346402#M46582</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;andreasruetten&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;I suggest you testing your custom board SWD connection on one more computer. if same connection error, we need to check SWD interface design. Thus refer this article please&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 27 Sep 2021 02:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54113-no-acces-via-SWD/m-p/1346402#M46582</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-09-27T02:48:02Z</dc:date>
    </item>
  </channel>
</rss>