<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFC Reader library - multiple RC663 on one LPC1769 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1345998#M46561</link>
    <description>&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;But there are parameters in the library&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_RS232&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_SPI&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_I2C&lt;/P&gt;&lt;P&gt;Doesn't this mean that I can use the reader library with RC663 connected via RS232?&lt;/P&gt;</description>
    <pubDate>Fri, 24 Sep 2021 18:13:01 GMT</pubDate>
    <dc:creator>DenisP</dc:creator>
    <dc:date>2021-09-24T18:13:01Z</dc:date>
    <item>
      <title>NFC Reader library - multiple RC663 on one LPC1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1344145#M46525</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Is it possible to connect multiple RC663 reader chips to different UARTs in LPC1769 using the Reader Library&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 14:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1344145#M46525</guid>
      <dc:creator>DenisP</dc:creator>
      <dc:date>2021-09-22T14:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Reader library - multiple RC663 on one LPC1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1344523#M46531</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The examples of the NFC Reader Library are for SPI communication. So the customer can't use the NFC Library via UART.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 02:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1344523#M46531</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-09-23T02:03:37Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Reader library - multiple RC663 on one LPC1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1345998#M46561</link>
      <description>&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;But there are parameters in the library&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_RS232&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_SPI&lt;/P&gt;&lt;P&gt;PHHAL_HW_BAL_CONNECTION_I2C&lt;/P&gt;&lt;P&gt;Doesn't this mean that I can use the reader library with RC663 connected via RS232?&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 18:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1345998#M46561</guid>
      <dc:creator>DenisP</dc:creator>
      <dc:date>2021-09-24T18:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Reader library - multiple RC663 on one LPC1769</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1346168#M46574</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, RC663 can supports RS232.&lt;/P&gt;
&lt;P&gt;Please find more information as the link.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com/docs/en/data-sheet/CLRC663.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/CLRC663.pdf&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;But the library supports SPI. If the customer needs RS232 and needs to design it themselves.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 26 Sep 2021 01:48:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NFC-Reader-library-multiple-RC663-on-one-LPC1769/m-p/1346168#M46574</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-09-26T01:48:30Z</dc:date>
    </item>
  </channel>
</rss>