<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Image not executed after transferring SB2.1 file in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1344982#M46541</link>
    <description>&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;thanks for the reply! Here is the command I used to generate the SB2.1 file:&lt;/P&gt;&lt;PRE&gt;elftosb -f lpc55xx -k "$sbkek" -c "config.bd" -o "$output" -s "$key" -S"$cert" -R "$cert" -h"$rkth" "$binary"&lt;/PRE&gt;&lt;P&gt;&lt;EM&gt;$binary&lt;/EM&gt; is the name of the binary file. The size of the binary file is ~ 17kB and the size of the SB2.1 file is ~ 20 kB, so it seems like the SB2.1 file contains the binary file.&lt;/P&gt;&lt;P&gt;What irritates me most is that even if I disable Secure Boot in the CMPA and flash an unsigned image, it is not executed any more.&amp;nbsp; Do you have any ideas why?&lt;/P&gt;&lt;P&gt;Best,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 09:39:12 GMT</pubDate>
    <dc:creator>rnk</dc:creator>
    <dc:date>2021-09-23T09:39:12Z</dc:date>
    <item>
      <title>Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1343408#M46501</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I encountered the following issue while testing Secure Boot on the LPC55S69 (revision 1b) following the&amp;nbsp;&lt;SPAN&gt;AN12283 guide:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Everything is working fine until the&amp;nbsp;SB2 file load step (§ 5.6.3).&amp;nbsp; After I executed the `receive-sb-file` command with my generated SB2.1 file and reset the chip, the firmware was not executed.&amp;nbsp; I am able to go back into ISP mode by activating the ISP pin and I can change the CMPA and CFPA configuration pages, erase the flash and flash new images, but none of the flashed images is actually executed after a reset.&amp;nbsp; Even if I erase the flash, the chip only boots into ISP mode if I also activate the ISP pin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am positive that the signature keys (ROTKH) are set up properly because flashing a signed image worked.&amp;nbsp; I also think that the SBKEK was setup correctly because the `receive-sb-file` command did not fail.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you know what could cause this behavior or how I can further debug it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;BR /&gt;Robin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PS: This is the .bd file that I used to generate the SB2.1 image:&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;options {
	flags = 0x8;
	buildNumber = 0x1;
	productVersion = "1.00.00";
	componentVersion = "1.00.00";
	secureBinaryVersion = "2.1";
}

sources {
	inputFile = extern(0);
}

section (0) {
	erase 0x0..0x40000;
	load inputFile &amp;gt; 0x0;
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 16:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1343408#M46501</guid>
      <dc:creator>rnk</dc:creator>
      <dc:date>2021-09-21T16:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1344949#M46540</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Robin,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please check in step&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;5.6.2 SB2 file creation, refer to the example for SB2.1:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1632388186641.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157056i0F6004DE9F424C5A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1632388186641.png" alt="Alice_Yang_0-1632388186641.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1632388186641.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Pay attention change the "input.bin" to the real name of your .bin file, and put the file in elftosb.exe path.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 09:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1344949#M46540</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-09-23T09:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1344982#M46541</link>
      <description>&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;thanks for the reply! Here is the command I used to generate the SB2.1 file:&lt;/P&gt;&lt;PRE&gt;elftosb -f lpc55xx -k "$sbkek" -c "config.bd" -o "$output" -s "$key" -S"$cert" -R "$cert" -h"$rkth" "$binary"&lt;/PRE&gt;&lt;P&gt;&lt;EM&gt;$binary&lt;/EM&gt; is the name of the binary file. The size of the binary file is ~ 17kB and the size of the SB2.1 file is ~ 20 kB, so it seems like the SB2.1 file contains the binary file.&lt;/P&gt;&lt;P&gt;What irritates me most is that even if I disable Secure Boot in the CMPA and flash an unsigned image, it is not executed any more.&amp;nbsp; Do you have any ideas why?&lt;/P&gt;&lt;P&gt;Best,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 09:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1344982#M46541</guid>
      <dc:creator>rnk</dc:creator>
      <dc:date>2021-09-23T09:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1345411#M46549</link>
      <description>&lt;P&gt;Hello Robin,&lt;/P&gt;
&lt;P&gt;1) Read CMPA out to check whether disabled Secure Boot successful.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2) Some other attentions:&lt;/P&gt;
&lt;P&gt;&amp;nbsp; the binary file $binary should be signed image.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The sbkek should loaded into device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 02:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1345411#M46549</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-09-24T02:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1347815#M46594</link>
      <description>&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;thanks for the hints!&lt;/P&gt;&lt;P&gt;re 1): According to the CMPA page, Secure Boot is disabled (see the attachment for the full configuration):&lt;/P&gt;&lt;PRE&gt;$ spsdk blhost -u 0x1fc9:0x0021 read-memory 0x9e400 512 cmpa.bin
$ spsdk pfr parse-binary --binary cmpa.bin --device lpc55s6x --type cmpa --output cmpa.txt
$ grep SEC_BOOT_EN: cmpa.txt
SEC_BOOT_EN: SECURE_BOOT_CFG_SEC_BOOT_EN_DISABLE # Width: 2b[0-3], Description: Secure boot enable&lt;/PRE&gt;&lt;P&gt;Flashing an unsigned image still does not work.&lt;/P&gt;&lt;P&gt;re 2):&lt;/P&gt;&lt;P&gt;I’ve set up the SBKEK and if I use a different SBKEK to generate the image, the receive-sb command fails, so I think that is working.&amp;nbsp; But indeed I’ve been using an unsigned image before.&amp;nbsp; (I assumed elftosb would add the signature when creating the SB2.1 file.)&amp;nbsp; Using the signed image makes the SB2.1 work on a different device, but my original chip is still stuck in the bootloader.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;&lt;SPAN&gt;Robin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Sep 2021 19:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1347815#M46594</guid>
      <dc:creator>rnk</dc:creator>
      <dc:date>2021-09-28T19:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1347949#M46598</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;re 1), does it can debug by IDE after change CMPA&amp;nbsp; Using "blhost -p COMxx write-memory 0x9E400 CMPA_empty.bin".?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can directly send the read back .bin file to me .&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 02:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1347949#M46598</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-09-29T02:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1348382#M46603</link>
      <description>&lt;P&gt;I’ve cleared the CMPA as suggested but that did not change the behavior.&amp;nbsp; I’ve attached the CMPA that I read out after clearing.&amp;nbsp; It looks like it has been cleared successfully.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 12:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1348382#M46603</guid>
      <dc:creator>rnk</dc:creator>
      <dc:date>2021-09-29T12:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: Image not executed after transferring SB2.1 file</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1352960#M46686</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I have checked your cmpa.bin , there is no problem, it disabled secure boot, it should be able to debug now, and able to configure secure boot again refer to AN12283 detail steps, pay attentions the points I mentioned :&lt;/P&gt;
&lt;P&gt;2) Some other attentions:&lt;/P&gt;
&lt;P&gt;the binary file $binary should be signed image.&lt;/P&gt;
&lt;P&gt;The sbkek should loaded into device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If not, sorry I also don't know the reason.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Sat, 09 Oct 2021 03:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Image-not-executed-after-transferring-SB2-1-file/m-p/1352960#M46686</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-10-09T03:03:08Z</dc:date>
    </item>
  </channel>
</rss>