<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CMOS camera interface LPC55(S)XX in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1344946#M46539</link>
    <description>&lt;P&gt;Hi Felipe&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to get the source code so I can make the required additions myself ?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Salman&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 09:07:37 GMT</pubDate>
    <dc:creator>muhammadsalmank</dc:creator>
    <dc:date>2021-09-23T09:07:37Z</dc:date>
    <item>
      <title>CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1339142#M46452</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;For our customer we are designing an image sensor with LTE-M/LPWAN integration. The camera needs to take still picture (320x2xx to 640x4xx pixels). As the solution need to be low cost we are looking into different solutions.&lt;/P&gt;&lt;P&gt;This document shows&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12868.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN12868.pdf&lt;/A&gt;&amp;nbsp;the integration of OV7673 with LPC55(S)XX via DVP interface but I am not able to find this library anywhere. Also I don't actually need to stream a video, only need to take single picture with no movement within the FOV.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has better options for a microcontroller (taking into account cost, complexity etc, open to DVP, MIPI-CSI or simple SPI) please let me know.&lt;/P&gt;&lt;P&gt;If anybody could help me make better decisions it would be highly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Salman&lt;/P&gt;</description>
      <pubDate>Mon, 13 Sep 2021 12:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1339142#M46452</guid>
      <dc:creator>muhammadsalmank</dc:creator>
      <dc:date>2021-09-13T12:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1340043#M46459</link>
      <description>&lt;P&gt;Hi Salman,&lt;/P&gt;
&lt;P&gt;You can find related software in this link: &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12868SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN12868SW.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 22:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1340043#M46459</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-09-14T22:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1340362#M46463</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. We need to take still pictures and from the API it looks like that wasn't the intention of this library. Is there an extended version of this library or API ? We are designing a low power device and it will be very handy to have more control over the camera output. For example I cannot find a Camera_Stop() function in the API.&lt;/P&gt;&lt;P&gt;Any help will be highly appreciated.&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;Salman&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 07:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1340362#M46463</guid>
      <dc:creator>muhammadsalmank</dc:creator>
      <dc:date>2021-09-15T07:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1342874#M46491</link>
      <description>&lt;P&gt;Hi Salman,&lt;/P&gt;
&lt;P&gt;Unfortunately, there is no extended version of this library. The API is described in application note. Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 17:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1342874#M46491</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-09-20T17:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1344946#M46539</link>
      <description>&lt;P&gt;Hi Felipe&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to get the source code so I can make the required additions myself ?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Salman&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 09:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1344946#M46539</guid>
      <dc:creator>muhammadsalmank</dc:creator>
      <dc:date>2021-09-23T09:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: CMOS camera interface LPC55(S)XX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1346039#M46566</link>
      <description>&lt;P&gt;Hi Salman,&lt;/P&gt;
&lt;P&gt;I am afraid source code is not available in our public website.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 20:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMOS-camera-interface-LPC55-S-XX/m-p/1346039#M46566</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-09-24T20:42:21Z</dc:date>
    </item>
  </channel>
</rss>