<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN11780 I2C Protocol and Configuration in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11780-I2C-Protocol-and-Configuration/m-p/1343011#M46497</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In AN11780, there is reference to "I2C-util.exe" which is used to interface with the SBL. Is the I2C protocol documented anywhere? I cannot seem to find it.&lt;/P&gt;&lt;P&gt;Secondly, is it possible to control other I2C parameters within the closed-source SBL, like adjusting I2C slave address or adjusting which I2C pins are utilized by the SBL?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 03:10:23 GMT</pubDate>
    <dc:creator>awseiger</dc:creator>
    <dc:date>2021-09-21T03:10:23Z</dc:date>
    <item>
      <title>AN11780 I2C Protocol and Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11780-I2C-Protocol-and-Configuration/m-p/1343011#M46497</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In AN11780, there is reference to "I2C-util.exe" which is used to interface with the SBL. Is the I2C protocol documented anywhere? I cannot seem to find it.&lt;/P&gt;&lt;P&gt;Secondly, is it possible to control other I2C parameters within the closed-source SBL, like adjusting I2C slave address or adjusting which I2C pins are utilized by the SBL?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 03:10:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN11780-I2C-Protocol-and-Configuration/m-p/1343011#M46497</guid>
      <dc:creator>awseiger</dc:creator>
      <dc:date>2021-09-21T03:10:23Z</dc:date>
    </item>
    <item>
      <title>Re: AN11780 I2C Protocol and Configuration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN11780-I2C-Protocol-and-Configuration/m-p/1343625#M46511</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181266" target="_self" aria-label="View Profile of awseiger"&gt;&lt;SPAN class=""&gt;awseiger&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;Sorry it&lt;SPAN&gt;&amp;nbsp;is not possible to get the source code of this application and &amp;nbsp;I2C protocol.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 03:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN11780-I2C-Protocol-and-Configuration/m-p/1343625#M46511</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-09-22T03:19:40Z</dc:date>
    </item>
  </channel>
</rss>