<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC51U68 Deep power down RTC</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1338741#M46450</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the deep-power-down function, I suppose that you have to add the line:&lt;/P&gt;
&lt;P&gt;SYSCON-&amp;gt;STARTERSET[0] |=&amp;nbsp;SYSCON_STARTER_RTC_MASK; &lt;/P&gt;
&lt;P&gt;BTW, pls follow up the deep power down waking-up procedure, I copied from UM11071.pdf, the deep-power down follows up Reset procedure rather than interrupt after waking-up:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;7.3.5 Deep power-down mode&lt;BR /&gt;In deep power-down mode, power and clocks are shut off to the entire chip with the&lt;BR /&gt;exception of the RTC.&lt;BR /&gt;During deep power-down mode, the contents of the SRAM and registers (other than those&lt;BR /&gt;in the RTC) are not retained. All functional pins are tri-stated in deep power-down mode&lt;BR /&gt;as long as chip power supplied externally.&lt;BR /&gt;7.3.5.1 Power configuration in deep power-down mode&lt;BR /&gt;Deep power-down mode has no configuration options. All clocks, the core, and all&lt;BR /&gt;peripherals are powered down. Only the RTC is powered, as long as power is supplied to&lt;BR /&gt;the device.&lt;BR /&gt;7.3.5.2 Wake-up from deep power-down mode:&lt;BR /&gt;Wake-up from deep power-down can be accomplished via the reset pin or the RTC.&lt;BR /&gt;7.3.5.3 Programming deep power-down mode using the RTC for wake-up:&lt;BR /&gt;The following steps must be performed to enter deep power-down mode when using the&lt;BR /&gt;RTC for waking up:&lt;BR /&gt;1. Set up the RTC high resolution timer. Write to the RTC VAL register. This starts the&lt;BR /&gt;high res timer if enabled. Another option is to use the 1 Hz alarm timer.&lt;BR /&gt;2. Call the power API function, see Chapter 8 “LPC51U68 Power profiles/Power control&lt;BR /&gt;API”.&lt;BR /&gt;7.3.5.4 Wake-up from deep power-down mode using the RTC:&lt;BR /&gt;The part goes through the entire reset process when the RTC times out:&lt;BR /&gt;• The PMU will turn on the on-chip voltage regulator. When the core voltage reaches&lt;BR /&gt;the power-on-reset (POR) trip point, a system reset will be triggered and the chip&lt;BR /&gt;boots.&lt;BR /&gt;• All registers will be in their reset state.&lt;/P&gt;
&lt;P&gt;Pls have a try.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 13 Sep 2021 03:01:01 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-09-13T03:01:01Z</dc:date>
    <item>
      <title>LPC51U68 Deep power down RTC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1338672#M46449</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I try to wake up DPD from RTC wake up timer or RTC Alarm. All my test seems not working.&lt;BR /&gt;Have you an example with RTC wake up please?&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;1 :&amp;nbsp; I inspire from SDK example (but it with button)&lt;BR /&gt;&lt;BR /&gt;2 : I configure with peripheral like this&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="capt.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/155793iAA956A56B8C22EEC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="capt.png" alt="capt.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;NB : the timer is enable by software after initialize alarm and time.&lt;/P&gt;&lt;P&gt;3: I try adding the few code below :&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SYSCON_RTCOSCCTRL_EN&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SYSCON_STARTER_RTC&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;RTC_EnableWakeUpTimerInterruptFromDPD&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;RTC&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;RTC_EnableAlarmTimerInterruptFromDPD&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;RTC&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;BR /&gt;I call like this :&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;RTC_SetWakeupCount&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;RTC_PERIPHERAL&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;RTC_WAKE_UP_TIME&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;POWER_EnterDeepPowerDown&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//&amp;nbsp;or&amp;nbsp;like&amp;nbsp;this&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//POWER_EnterDeepPowerDown(SYSCON_PDRUNCFG_PDEN_SRAMX_MASK&amp;nbsp;|&amp;nbsp;SYSCON_PDRUNCFG_PDEN_SRAM0_MASK);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4 : I understand that Wakeupcount is onetime use.that why I reinit it before enter DPD&lt;/P&gt;&lt;P&gt;5 : the RTC_IRQHAndler work with wakeup or alarm before I call EnterDeepPowerDown.&lt;/P&gt;&lt;P&gt;thanks for help.&lt;/P&gt;&lt;P&gt;Benoit&lt;/P&gt;</description>
      <pubDate>Sun, 12 Sep 2021 20:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1338672#M46449</guid>
      <dc:creator>Benoit2</dc:creator>
      <dc:date>2021-09-12T20:54:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 Deep power down RTC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1338741#M46450</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the deep-power-down function, I suppose that you have to add the line:&lt;/P&gt;
&lt;P&gt;SYSCON-&amp;gt;STARTERSET[0] |=&amp;nbsp;SYSCON_STARTER_RTC_MASK; &lt;/P&gt;
&lt;P&gt;BTW, pls follow up the deep power down waking-up procedure, I copied from UM11071.pdf, the deep-power down follows up Reset procedure rather than interrupt after waking-up:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;7.3.5 Deep power-down mode&lt;BR /&gt;In deep power-down mode, power and clocks are shut off to the entire chip with the&lt;BR /&gt;exception of the RTC.&lt;BR /&gt;During deep power-down mode, the contents of the SRAM and registers (other than those&lt;BR /&gt;in the RTC) are not retained. All functional pins are tri-stated in deep power-down mode&lt;BR /&gt;as long as chip power supplied externally.&lt;BR /&gt;7.3.5.1 Power configuration in deep power-down mode&lt;BR /&gt;Deep power-down mode has no configuration options. All clocks, the core, and all&lt;BR /&gt;peripherals are powered down. Only the RTC is powered, as long as power is supplied to&lt;BR /&gt;the device.&lt;BR /&gt;7.3.5.2 Wake-up from deep power-down mode:&lt;BR /&gt;Wake-up from deep power-down can be accomplished via the reset pin or the RTC.&lt;BR /&gt;7.3.5.3 Programming deep power-down mode using the RTC for wake-up:&lt;BR /&gt;The following steps must be performed to enter deep power-down mode when using the&lt;BR /&gt;RTC for waking up:&lt;BR /&gt;1. Set up the RTC high resolution timer. Write to the RTC VAL register. This starts the&lt;BR /&gt;high res timer if enabled. Another option is to use the 1 Hz alarm timer.&lt;BR /&gt;2. Call the power API function, see Chapter 8 “LPC51U68 Power profiles/Power control&lt;BR /&gt;API”.&lt;BR /&gt;7.3.5.4 Wake-up from deep power-down mode using the RTC:&lt;BR /&gt;The part goes through the entire reset process when the RTC times out:&lt;BR /&gt;• The PMU will turn on the on-chip voltage regulator. When the core voltage reaches&lt;BR /&gt;the power-on-reset (POR) trip point, a system reset will be triggered and the chip&lt;BR /&gt;boots.&lt;BR /&gt;• All registers will be in their reset state.&lt;/P&gt;
&lt;P&gt;Pls have a try.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 13 Sep 2021 03:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1338741#M46450</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-09-13T03:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 Deep power down RTC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1339259#M46454</link>
      <description>&lt;P&gt;Hello XiangJun Rong,&lt;/P&gt;&lt;P&gt;thanks for helping.&lt;BR /&gt;The problem was hardware. I don't know why.&lt;/P&gt;&lt;P&gt;for informations :&lt;BR /&gt;my last settings are :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="capt2.png" style="width: 928px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/155916i4AE37FED99F50034/image-size/large?v=v2&amp;amp;px=999" role="button" title="capt2.png" alt="capt2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and to go to DPD:&lt;BR /&gt;&lt;BR /&gt;RTC_EnableWakeUpTimerInterruptFromDPD(RTC,1);&lt;BR /&gt;RTC_SetWakeupCount(RTC, 6000);&lt;BR /&gt;POWER_EnterDeepPowerDown(0);&lt;/P&gt;&lt;P&gt;I don't need to do this :&lt;/P&gt;&lt;P&gt;SYSCON-&amp;gt;STARTERSET[0] |= SYSCON_STARTER_RTC_MASK;&lt;BR /&gt;according datasheet "Deep power-down mode has no configuration options"&lt;BR /&gt;&lt;BR /&gt;Many thanks for help.&lt;/P&gt;&lt;P&gt;kind regards,&lt;BR /&gt;Benoit&lt;/P&gt;</description>
      <pubDate>Mon, 13 Sep 2021 19:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-Deep-power-down-RTC/m-p/1339259#M46454</guid>
      <dc:creator>Benoit2</dc:creator>
      <dc:date>2021-09-13T19:17:24Z</dc:date>
    </item>
  </channel>
</rss>