<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S16 SPI SDK code not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-SDK-code-not-working/m-p/1337918#M46441</link>
    <description>&lt;P&gt;Hello amulya0129,&lt;/P&gt;
&lt;P&gt;My apologies for the delay. Is the problem still present? I would recommend testing with one of the SPI examples from the SDK. These do need JP20 and JP21 in place.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
    <pubDate>Thu, 09 Sep 2021 21:03:23 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2021-09-09T21:03:23Z</dc:date>
    <item>
      <title>LPC55S16 SPI SDK code not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-SDK-code-not-working/m-p/1330413#M46303</link>
      <description>&lt;P&gt;Hi, Im working on to LPC55S16-evk board. i have LPC55S16 board set as master and STM32F429ZI development board as slave. im using SDK Code with no changes. still i receive only junk on stm32f429zi board. i checked in loopback, the communication works fine.&amp;nbsp; I had faced the similar issue wrt UART but later i found the jumper JP12 has to be installed. is there anything im missing in SPI like jumper installation or any other issue? Please help&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 13:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-SDK-code-not-working/m-p/1330413#M46303</guid>
      <dc:creator>amulya0129</dc:creator>
      <dc:date>2021-08-26T13:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16 SPI SDK code not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-SDK-code-not-working/m-p/1337918#M46441</link>
      <description>&lt;P&gt;Hello amulya0129,&lt;/P&gt;
&lt;P&gt;My apologies for the delay. Is the problem still present? I would recommend testing with one of the SPI examples from the SDK. These do need JP20 and JP21 in place.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 21:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-SPI-SDK-code-not-working/m-p/1337918#M46441</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-09-09T21:03:23Z</dc:date>
    </item>
  </channel>
</rss>