<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IEC60730 library for LPC54113 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1333040#M46357</link>
    <description>&lt;P&gt;But no IEC60730 library for LPC54113 in the link provided.&lt;/P&gt;&lt;P&gt;Is it possible to get the source code if we agree to sign an NDA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Sep 2021 08:07:51 GMT</pubDate>
    <dc:creator>conradkwok</dc:creator>
    <dc:date>2021-09-01T08:07:51Z</dc:date>
    <item>
      <title>IEC60730 library for LPC54113</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1332437#M46346</link>
      <description>&lt;P&gt;I don't think IEC60730 library is available for LPC54113 yet.&lt;BR /&gt;On the other hand, IEC60730 library is available for LPC51U68.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Since LPC54113 and LPC51U68 are basically the same except that the CPU core is M4 and M0 respectively. I think it should be easy to adapt the LPC51U68 version of the library for use with LPC54113 if I have the source code.&lt;/P&gt;&lt;P&gt;Where can I get the source code of the LPC51U68 version of the library?&lt;/P&gt;&lt;P&gt;Thank you very much in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 09:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1332437#M46346</guid>
      <dc:creator>conradkwok</dc:creator>
      <dc:date>2021-08-31T09:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: IEC60730 library for LPC54113</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1332850#M46352</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;We can get library test code here&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/product-information/nxp-product-programs/iec-60730-safety-standard-for-household-appliances:APIEC60730?tid=redAPIEC60730_2" target="_blank"&gt;https://www.nxp.com/products/product-information/nxp-product-programs/iec-60730-safety-standard-for-household-appliances:APIEC60730?tid=redAPIEC60730_2&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;But the library source code is not open to external.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 03:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1332850#M46352</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-09-01T03:48:17Z</dc:date>
    </item>
    <item>
      <title>Re: IEC60730 library for LPC54113</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1333040#M46357</link>
      <description>&lt;P&gt;But no IEC60730 library for LPC54113 in the link provided.&lt;/P&gt;&lt;P&gt;Is it possible to get the source code if we agree to sign an NDA?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Sep 2021 08:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1333040#M46357</guid>
      <dc:creator>conradkwok</dc:creator>
      <dc:date>2021-09-01T08:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: IEC60730 library for LPC54113</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1333651#M46372</link>
      <description>&lt;P&gt;Please provide us your application name. I will check if it's possible internally.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 02:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IEC60730-library-for-LPC54113/m-p/1333651#M46372</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-09-02T02:02:34Z</dc:date>
    </item>
  </channel>
</rss>