<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC18xxJET100 - SDRAM DQM Signal missing? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330555#M46308</link>
    <description>&lt;P&gt;The design in question would be using an 8bit wide data bus, but the SDRAM chip still has the DQM signal, which if I understand correctly affects write/read operations.&lt;/P&gt;&lt;P&gt;SDRAM Part Zentel&amp;nbsp;A3V56S30GTP-60&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dqm.PNG" style="width: 851px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/154250i66FED7E09A8E7F7B/image-size/large?v=v2&amp;amp;px=999" role="button" title="dqm.PNG" alt="dqm.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;dqm.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 19:41:48 GMT</pubDate>
    <dc:creator>urosg</dc:creator>
    <dc:date>2021-08-26T19:41:48Z</dc:date>
    <item>
      <title>LPC18xxJET100 - SDRAM DQM Signal missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1329407#M46272</link>
      <description>&lt;P&gt;I am working on a new design where I would like to use external SDRAM memory with the LPC1833JET100 (TFBGA100 package) part because we already use it in our other products, but all without external RAM.&lt;/P&gt;&lt;P&gt;While preparing schematics and going through signals I am missing a EMC_DQMOUT[0:3] signal on the TFBA100 package, is there a way to repurpose OE signal for example for this function as OE signal is not used in SDRAM configuration only in SRAM configurations.&lt;/P&gt;&lt;P&gt;Since there is a missing DQM signal is it even possible to use SDRAM with LPC18xx in TFBGA100 package or am I stuck with SRAM only?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any insight!&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 11:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1329407#M46272</guid>
      <dc:creator>urosg</dc:creator>
      <dc:date>2021-08-25T11:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC18xxJET100 - SDRAM DQM Signal missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330061#M46292</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;As you know that the EMC_DQM[0:3] are output signals from EMC module of LPC, they are used to select Byte lane of SDRAM.&lt;/P&gt;
&lt;P&gt;For your current design, can you tell us the data width of SDRAM, if you use 8 bits data width, you do not need connect the DQM signal, if you use 16/32 data width, how do you connect the DQM pins of SDRAM at the time being?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 06:23:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330061#M46292</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-08-26T06:23:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC18xxJET100 - SDRAM DQM Signal missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330555#M46308</link>
      <description>&lt;P&gt;The design in question would be using an 8bit wide data bus, but the SDRAM chip still has the DQM signal, which if I understand correctly affects write/read operations.&lt;/P&gt;&lt;P&gt;SDRAM Part Zentel&amp;nbsp;A3V56S30GTP-60&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dqm.PNG" style="width: 851px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/154250i66FED7E09A8E7F7B/image-size/large?v=v2&amp;amp;px=999" role="button" title="dqm.PNG" alt="dqm.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;dqm.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 19:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330555#M46308</guid>
      <dc:creator>urosg</dc:creator>
      <dc:date>2021-08-26T19:41:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC18xxJET100 - SDRAM DQM Signal missing?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330708#M46314</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I see your issue, the EMC module of&amp;nbsp; LPC18xxJET100 with 100 pins does not have DQM pin, but the DQM function is required for the Zentel A3V56S30GTP-60 SDRAM, so I do not think the DQM pin of SDRAM can be connected to a fixed logic. So I do not think you can connect SDRAM because of lack of DQM pin for the LPC18xxJET100 .&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 03:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC18xxJET100-SDRAM-DQM-Signal-missing/m-p/1330708#M46314</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-08-27T03:21:39Z</dc:date>
    </item>
  </channel>
</rss>