<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックFlag Interrupt of CTIMER on LPC845</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flag-Interrupt-of-CTIMER-on-LPC845/m-p/1330496#M46306</link>
    <description>&lt;P&gt;hi&lt;BR /&gt;I have set the CTIMER peripheral of the LPC845 to read 3 pulses via cap0 cap1 and cap2. I have set the CCR register to trigger the interrupt on both rising and falling edges. How do I detect the type of interrupt that was triggered, whether falling or rising?&amp;nbsp; I haven't found any register for this.&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 16:15:26 GMT</pubDate>
    <dc:creator>anto</dc:creator>
    <dc:date>2021-08-26T16:15:26Z</dc:date>
    <item>
      <title>Flag Interrupt of CTIMER on LPC845</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flag-Interrupt-of-CTIMER-on-LPC845/m-p/1330496#M46306</link>
      <description>&lt;P&gt;hi&lt;BR /&gt;I have set the CTIMER peripheral of the LPC845 to read 3 pulses via cap0 cap1 and cap2. I have set the CCR register to trigger the interrupt on both rising and falling edges. How do I detect the type of interrupt that was triggered, whether falling or rising?&amp;nbsp; I haven't found any register for this.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 16:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flag-Interrupt-of-CTIMER-on-LPC845/m-p/1330496#M46306</guid>
      <dc:creator>anto</dc:creator>
      <dc:date>2021-08-26T16:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flag Interrupt of CTIMER on LPC845</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flag-Interrupt-of-CTIMER-on-LPC845/m-p/1330744#M46316</link>
      <description>&lt;P&gt;Hello anto,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry there isn't the register. Some suggestions:&lt;/P&gt;
&lt;P&gt;how about read the signal high/low in interrupt function.&lt;/P&gt;
&lt;P&gt;or&amp;nbsp; the initialize state is know, then through the interrupt number judge rising or falling.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;or Use SCtimer six capture, CAP0 control signal 1 rising, CAP1 control signal1 falling.&amp;nbsp; CAP2 control signal 2rising, CAP3 control signal2 falling.&amp;nbsp; CAP4 control signal 3 rising, CAP5 control signal3 falling.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 04:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flag-Interrupt-of-CTIMER-on-LPC845/m-p/1330744#M46316</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-27T04:19:39Z</dc:date>
    </item>
  </channel>
</rss>