<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1850/LPC1857/LPC4350/LPC4357 compatible on MYIR's boards</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1850-LPC1857-LPC4350-LPC4357-compatible-on-MYIR-s-boards/m-p/1329993#M46288</link>
    <description>&lt;P&gt;Does the LPC4350FET256 work with the same binaries as the LPC1850FET256?&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 05:02:44 GMT</pubDate>
    <dc:creator>SU1</dc:creator>
    <dc:date>2021-08-26T05:02:44Z</dc:date>
    <item>
      <title>LPC1850/LPC1857/LPC4350/LPC4357 compatible on MYIR's boards</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1850-LPC1857-LPC4350-LPC4357-compatible-on-MYIR-s-boards/m-p/525160#M7796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lz6661 on Mon Nov 18 23:59:45 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fhttp%3A%2F%2Fwww.myirtech.com" rel="nofollow" target="_blank"&gt;&lt;STRONG&gt;MYIR&lt;/STRONG&gt;&lt;/A&gt;&lt;SPAN&gt; offers &lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fhttp%3A%2F%2Fwww.myirtech.com%2Flist.asp%3Fid%3D422" rel="nofollow" target="_blank"&gt;&lt;STRONG&gt;MYD-LPC435X&lt;/STRONG&gt;&lt;/A&gt;&lt;SPAN&gt; and &lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fhttp%3A%2F%2Fwww.myirtech.com%2Flist.asp%3Fid%3D430" rel="nofollow" target="_blank"&gt;&lt;STRONG&gt;MYD-LPC185X&lt;/STRONG&gt;&lt;/A&gt;&lt;SPAN&gt; Development Boards, the boards are using the same circuit design with minor configuration settings. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;[img]&lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.myirtech.com%2Fattached%2Fimage%2F20131022%2FMYD-LPC435X_185X.jpg%5B%2Fimg%5D" rel="nofollow" target="_blank"&gt;http://www.myirtech.com/attached/image/20131022/MYD-LPC435X_185X.jpg[/img]&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP LPC1850FET256 / LPC1857FET256 / LPC4350FET256 / LPC4357FET256 (pin-to-pin compatible on board)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;NXP LPC4350 FET256 / LPC4357FET256&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;- 204 MHz, 32-bit ARM Cortex-M4 processor&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 204 MHz, 32-bit ARM Cortex-M0 asymmetrical coprocessor&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Up to 1 MB on-chip dual bank flash memory with flash accelerator (only for LPC4357)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SRAM for code and data use (136 kB for LPC4357, 264 kB for LPC4350)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 32 kB ROM containing boot code and on-chip software drivers&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 32 bit One-Time Programmable (OTP) memory for customer use&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;NXP LPC1850FET256 / LPC1857FET256&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;- ARM Cortex-M3 processor, running at CPU frequencies of up to 180 MHz &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- SRAM for code and data use (136 kB for LPC1857, 200kB for LPC1850) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- ROM containing boot code and on-chip software drivers (64kB for LPC1857, 32kB for LPC1850)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Up to 1 MB on-chip dual bank flash memory with flash accelerator (only for LPC1857) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 16 kB on-chip EEPROM data memory (only for LPC1857)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Other Features&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;- 32MB SDRAM&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 2MB Nor Flash&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 4MB SPI Data FLASH&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 3 x UART (UART0, UART2 and UART3, UART2 need external MAX3232)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x USB Host and 1 x USB OTG&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x Ethernet&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 2 x CAN&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x RS485 (reused with UART2)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Audio Input/Output&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x Micro SD card slot&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x LCD interface (4.3- or 7- inch LCD for option)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x resistive touch screen interface&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- 1 x JTAG&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- DC5V or USB power supply&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- MDK-ARM sample source code&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 18:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1850-LPC1857-LPC4350-LPC4357-compatible-on-MYIR-s-boards/m-p/525160#M7796</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T18:15:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1850/LPC1857/LPC4350/LPC4357 compatible on MYIR's boards</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1850-LPC1857-LPC4350-LPC4357-compatible-on-MYIR-s-boards/m-p/1329993#M46288</link>
      <description>&lt;P&gt;Does the LPC4350FET256 work with the same binaries as the LPC1850FET256?&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 05:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1850-LPC1857-LPC4350-LPC4357-compatible-on-MYIR-s-boards/m-p/1329993#M46288</guid>
      <dc:creator>SU1</dc:creator>
      <dc:date>2021-08-26T05:02:44Z</dc:date>
    </item>
  </channel>
</rss>