<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: CAN Implementation using lpc1768</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1328663#M46260</link>
    <description>&lt;P&gt;&lt;EM&gt;&amp;gt; register is set to the value 0x21 I am seeing can mode getting set to reboot and ICR register is having 0x0030000 values which is nothing but start of frame error.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I suppose that would point to a hardware issue. I am not very proficient with the LPC176x CAN peripherla, though.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;A CAN node creates an error when it is unable to get a message out, e.g. there is no other device on the bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;You can try loopback mode (connect Tx and Rx, not sure if it's directly supported by the LPC176x), or connect two devices directly on board logic level (Rx-&amp;gt;Tx, Tx-&amp;gt;Rx, and GND).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hi Nxp support team, ...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;While some NXP staff members are active here, a lot of posters (like me) are NXP users and volunteers, and not affiliated with NXP. This is an open forum, hosted by NXP.&lt;/P&gt;&lt;P&gt;The main difference is, no answer guaranteed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Aug 2021 13:06:26 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2021-08-24T13:06:26Z</dc:date>
    <item>
      <title>CAN Implementation using lpc1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1328474#M46258</link>
      <description>&lt;P&gt;Hi Nxp support team,&lt;/P&gt;&lt;P&gt;I am trying to use lcp1768 is normal operation mode and transmit a CAN message through it.&lt;/P&gt;&lt;P&gt;currently I am facing transmit error issue whenever I try to transmit a message.&lt;/P&gt;&lt;P&gt;i.e as soon as LPC_CAN1-&amp;gt;CMR = 0x21; register is set to the value 0x21 I am seeing can mode getting set to reboot and ICR register is having 0x0030000 values which is nothing but start of frame error.&lt;/P&gt;&lt;P&gt;hardware connections&lt;/P&gt;&lt;P&gt;From LPC1768 i am connecting CAN1 tx to mcp2551 tx and LPC1768 rx i am connecting it to mcp2551 rx .&lt;/P&gt;&lt;P&gt;Currently i am using coocox ide and i have attached my complete project .&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know where is the problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 09:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1328474#M46258</guid>
      <dc:creator>Mithunv</dc:creator>
      <dc:date>2021-08-24T09:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Implementation using lpc1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1328663#M46260</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; register is set to the value 0x21 I am seeing can mode getting set to reboot and ICR register is having 0x0030000 values which is nothing but start of frame error.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I suppose that would point to a hardware issue. I am not very proficient with the LPC176x CAN peripherla, though.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;A CAN node creates an error when it is unable to get a message out, e.g. there is no other device on the bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;You can try loopback mode (connect Tx and Rx, not sure if it's directly supported by the LPC176x), or connect two devices directly on board logic level (Rx-&amp;gt;Tx, Tx-&amp;gt;Rx, and GND).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hi Nxp support team, ...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;While some NXP staff members are active here, a lot of posters (like me) are NXP users and volunteers, and not affiliated with NXP. This is an open forum, hosted by NXP.&lt;/P&gt;&lt;P&gt;The main difference is, no answer guaranteed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 13:06:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1328663#M46260</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-08-24T13:06:26Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Implementation using lpc1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1330652#M46311</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Mithunv,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;First confirm, h&lt;/SPAN&gt;&lt;SPAN&gt;ave you connect to another CAN Node with your LPC1768 CAN?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is CAN demo based on lpc1769 under LPCopen, recommend you first to refer to.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc17xx:LPCOPEN-SOFTWARE-FOR-LPC17XX" target="_blank"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc17xx:LPCOPEN-SOFTWARE-FOR-LPC17XX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 27 Aug 2021 01:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-Implementation-using-lpc1768/m-p/1330652#M46311</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-27T01:34:13Z</dc:date>
    </item>
  </channel>
</rss>