<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB tethering (USB Host RNDIS and LwIP) using LPC55 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1328178#M46246</link>
    <description>&lt;P&gt;Do you have the demo for USB RNDIS slave for PC ?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Aug 2021 03:39:09 GMT</pubDate>
    <dc:creator>andarm</dc:creator>
    <dc:date>2021-08-24T03:39:09Z</dc:date>
    <item>
      <title>USB tethering (USB Host RNDIS and LwIP) using LPC55</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1209839#M43528</link>
      <description>&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;I'm working on a product using a LPC55S69 running with FreeRTOS, AWS IoT and lwip IP stack. Now I would like to connect the board to internet using an Android phone with USB connection tethering. I think the USB Host CDC RNDIS example from the SDK middleware library is the good starting point.&lt;/P&gt;&lt;P&gt;Is there any example of how to connect LwIP to USB Host CDC RNDIS library for LPC55?&lt;/P&gt;&lt;P&gt;I've heard about an example called "usb_ethernetif_freertos.c" but not sure it will be compatible. (&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/td-p/1194463" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/LwIP-and-USB-device/td-p/1194463&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;Thanks in advance and bests regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 19:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1209839#M43528</guid>
      <dc:creator>Michael_25</dc:creator>
      <dc:date>2021-01-11T19:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB tethering (USB Host RNDIS and LwIP) using LPC55</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1210164#M43538</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It's possible but there is no demo for LPC55.&lt;/P&gt;
&lt;P&gt;We have&amp;nbsp;lwip_dhcp_usb demo under LPC54xxx SDK and imx RT SDK. This demo&amp;nbsp;describes how to use the USB Host RNDIS &amp;amp; LWIP&amp;nbsp; to access the internet via a Android cellphone which turns on the USB tethering function.&lt;/P&gt;
&lt;P&gt;You can refer it and porting it to LPC55.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 07:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1210164#M43538</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-01-12T07:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: USB tethering (USB Host RNDIS and LwIP) using LPC55</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1328178#M46246</link>
      <description>&lt;P&gt;Do you have the demo for USB RNDIS slave for PC ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 03:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-tethering-USB-Host-RNDIS-and-LwIP-using-LPC55/m-p/1328178#M46246</guid>
      <dc:creator>andarm</dc:creator>
      <dc:date>2021-08-24T03:39:09Z</dc:date>
    </item>
  </channel>
</rss>