<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB-HS logical endpoints</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-HS-logical-endpoints/m-p/1327987#M46242</link>
    <description>&lt;P&gt;My logical endpoints map for USB-HS is:&lt;/P&gt;&lt;P&gt;EP1 - CDC1 Interrupt&lt;/P&gt;&lt;P&gt;EP2 - CDC2 interrupt&lt;/P&gt;&lt;P&gt;EP3 - CDC1 BULK IN/OUT&lt;/P&gt;&lt;P&gt;EP4 - CDC2 BULK IN/OUT&lt;/P&gt;&lt;P&gt;EP5 - HID BULK IN/OUT&lt;/P&gt;&lt;P&gt;I'm trying to add a MSC using EP6, but it doesn't work with this EP (works with lower EPs if I cancel another interface).&lt;/P&gt;&lt;P&gt;I'm using LPC55S16-EVK, and the solution should work with&amp;nbsp;&lt;SPAN&gt;LPC5514JBD64E as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm trying to understand if I ran out of endpoints, or the problem has nothing to do with that.&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;page 57,&lt;/P&gt;&lt;P&gt;USB-HS :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt; Supports 8 physical (16 logical) endpoints with up to 8 kB endpoint buffer RAM. &lt;/LI-CODE&gt;&lt;P&gt;So I just want to make sure that it should work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 23 Aug 2021 19:26:21 GMT</pubDate>
    <dc:creator>embedded_eng_</dc:creator>
    <dc:date>2021-08-23T19:26:21Z</dc:date>
    <item>
      <title>USB-HS logical endpoints</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-HS-logical-endpoints/m-p/1327987#M46242</link>
      <description>&lt;P&gt;My logical endpoints map for USB-HS is:&lt;/P&gt;&lt;P&gt;EP1 - CDC1 Interrupt&lt;/P&gt;&lt;P&gt;EP2 - CDC2 interrupt&lt;/P&gt;&lt;P&gt;EP3 - CDC1 BULK IN/OUT&lt;/P&gt;&lt;P&gt;EP4 - CDC2 BULK IN/OUT&lt;/P&gt;&lt;P&gt;EP5 - HID BULK IN/OUT&lt;/P&gt;&lt;P&gt;I'm trying to add a MSC using EP6, but it doesn't work with this EP (works with lower EPs if I cancel another interface).&lt;/P&gt;&lt;P&gt;I'm using LPC55S16-EVK, and the solution should work with&amp;nbsp;&lt;SPAN&gt;LPC5514JBD64E as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm trying to understand if I ran out of endpoints, or the problem has nothing to do with that.&lt;/P&gt;&lt;P&gt;According to&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/nxp/data-sheets/LPC55S1x_PDS.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;page 57,&lt;/P&gt;&lt;P&gt;USB-HS :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt; Supports 8 physical (16 logical) endpoints with up to 8 kB endpoint buffer RAM. &lt;/LI-CODE&gt;&lt;P&gt;So I just want to make sure that it should work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 19:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-HS-logical-endpoints/m-p/1327987#M46242</guid>
      <dc:creator>embedded_eng_</dc:creator>
      <dc:date>2021-08-23T19:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: USB-HS logical endpoints</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-HS-logical-endpoints/m-p/1328248#M46251</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;embedded_eng_,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It seems there is some issue in DS.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The USB-HS of lpc55s16&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Supports 12 physical (6 logical) endpoints including control endpoints.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 05:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-HS-logical-endpoints/m-p/1328248#M46251</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-24T05:55:54Z</dc:date>
    </item>
  </channel>
</rss>