<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProgramatic way to determine which LPC43x0 I'm running on</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326493#M46215</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I thought there would be a device register I could query to determine the flavor of LPC43x0 my application is running on. I could not find it in the datasheet. What's the best way for the application to determine this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Todd&lt;/P&gt;</description>
    <pubDate>Thu, 19 Aug 2021 22:49:48 GMT</pubDate>
    <dc:creator>tmullanix</dc:creator>
    <dc:date>2021-08-19T22:49:48Z</dc:date>
    <item>
      <title>Programatic way to determine which LPC43x0 I'm running on</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326493#M46215</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I thought there would be a device register I could query to determine the flavor of LPC43x0 my application is running on. I could not find it in the datasheet. What's the best way for the application to determine this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Todd&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 22:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326493#M46215</guid>
      <dc:creator>tmullanix</dc:creator>
      <dc:date>2021-08-19T22:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: Programatic way to determine which LPC43x0 I'm running on</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326567#M46217</link>
      <description>&lt;P&gt;Hi, Todd,&lt;/P&gt;
&lt;P&gt;For the flashless LPC43xx family for example LPC43x0, the IAP commands are not supported, but the ISP commands are supported.&lt;/P&gt;
&lt;P&gt;You can use ISP commands to read the part identification number with the following commands J, but it is not possible to read a register to get the ID or to execute a function in IAP, because IAP is not supported for flashless part.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1629426567318.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153515i499702EF2600D1C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1629426567318.png" alt="xiangjun_rong_0-1629426567318.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1629426567318.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 02:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326567#M46217</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-08-20T02:32:59Z</dc:date>
    </item>
    <item>
      <title>Re: Programatic way to determine which LPC43x0 I'm running on</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326613#M46219</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply. Which document did the table you attached come from?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Todd&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 03:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326613#M46219</guid>
      <dc:creator>tmullanix</dc:creator>
      <dc:date>2021-08-20T03:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: Programatic way to determine which LPC43x0 I'm running on</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326627#M46220</link>
      <description>&lt;P&gt;Hi, Todd,&lt;/P&gt;
&lt;P&gt;I refer to UM10503.pdf, which can be downloaded from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc4300-cortex-m4-m0/high-performance-32-bit-microcontroller-mcu-based-on-arm-cortex-m4-m0-cores:LPC4317JET100?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc4300-cortex-m4-m0/high-performance-32-bit-microcontroller-mcu-based-on-arm-cortex-m4-m0-cores:LPC4317JET100?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 05:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Programatic-way-to-determine-which-LPC43x0-I-m-running-on/m-p/1326627#M46220</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-08-20T05:01:39Z</dc:date>
    </item>
  </channel>
</rss>