<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックablout Master Security Wrapper(MSW)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ablout-Master-Security-Wrapper-MSW/m-p/1326168#M46211</link>
    <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Is there any more information about&amp;nbsp;Master Security Wrapper(MSW)?&amp;nbsp; In UM11126 I only find below.&lt;/P&gt;&lt;P&gt;&amp;nbsp; where is it? How to set it and modify it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;&amp;nbsp;47.3.3.3 Master Security Wrapper (MSW)&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;TrustZone for ARMv8-M offers IDAU functionality for CM33 when TrustZone feature is&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;configured. However, IDAU is not available for all other masters on LPC55S6x. A special&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;wrapper Master Security Wrapper (MSW) is implemented for each AHB Master except&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;CPU0.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;MSW allows application to set security attribute for each master. There are two categories&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;of the MSW:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;1. Simple Master: Bus Masters that can perform data access only: SDIO, USB-FS,&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;DMA0, DMA1, Hash-AES.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;MSW for simple master enables strict checking by default. Secure data accesses can&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;access secure memory only. A programmable option to disable strict checking allows data&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;access from secure master to Non-secure memory.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; thanks a lot !&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 19 Aug 2021 09:26:32 GMT</pubDate>
    <dc:creator>superliyou</dc:creator>
    <dc:date>2021-08-19T09:26:32Z</dc:date>
    <item>
      <title>ablout Master Security Wrapper(MSW)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ablout-Master-Security-Wrapper-MSW/m-p/1326168#M46211</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Is there any more information about&amp;nbsp;Master Security Wrapper(MSW)?&amp;nbsp; In UM11126 I only find below.&lt;/P&gt;&lt;P&gt;&amp;nbsp; where is it? How to set it and modify it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;&amp;nbsp;47.3.3.3 Master Security Wrapper (MSW)&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;TrustZone for ARMv8-M offers IDAU functionality for CM33 when TrustZone feature is&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;configured. However, IDAU is not available for all other masters on LPC55S6x. A special&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;wrapper Master Security Wrapper (MSW) is implemented for each AHB Master except&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;CPU0.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;MSW allows application to set security attribute for each master. There are two categories&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;of the MSW:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;1. Simple Master: Bus Masters that can perform data access only: SDIO, USB-FS,&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;DMA0, DMA1, Hash-AES.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;MSW for simple master enables strict checking by default. Secure data accesses can&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;access secure memory only. A programmable option to disable strict checking allows data&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;EM&gt;access from secure master to Non-secure memory.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; thanks a lot !&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 09:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ablout-Master-Security-Wrapper-MSW/m-p/1326168#M46211</guid>
      <dc:creator>superliyou</dc:creator>
      <dc:date>2021-08-19T09:26:32Z</dc:date>
    </item>
    <item>
      <title>Re: ablout Master Security Wrapper(MSW)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ablout-Master-Security-Wrapper-MSW/m-p/1327903#M46240</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can check all master security level (MSW) settings in the &lt;STRONG&gt;47.4.73 Master secure level register&lt;/STRONG&gt; section of the UM. Additionally, you can check the TrustZone examples included in our MCUXpresso SDK.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 15:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ablout-Master-Security-Wrapper-MSW/m-p/1327903#M46240</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-08-23T15:59:23Z</dc:date>
    </item>
  </channel>
</rss>