<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1768 ac as USB device in low speed</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-ac-as-USB-device-in-low-speed/m-p/1325571#M46195</link>
    <description>&lt;P&gt;I have an LPC1768 acting as a USB device to a host using USB 2.0.&lt;/P&gt;&lt;P&gt;It currently connects at the fullspeed (12mbps).&lt;/P&gt;&lt;P&gt;I want to configure the device/LPC1768 to use low speed(1.5 mbps).&lt;/P&gt;&lt;P&gt;I cannot find where this is configured if at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a register to change the USB speed to use low speed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
    <pubDate>Wed, 18 Aug 2021 16:03:27 GMT</pubDate>
    <dc:creator>enpingado</dc:creator>
    <dc:date>2021-08-18T16:03:27Z</dc:date>
    <item>
      <title>LPC1768 ac as USB device in low speed</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-ac-as-USB-device-in-low-speed/m-p/1325571#M46195</link>
      <description>&lt;P&gt;I have an LPC1768 acting as a USB device to a host using USB 2.0.&lt;/P&gt;&lt;P&gt;It currently connects at the fullspeed (12mbps).&lt;/P&gt;&lt;P&gt;I want to configure the device/LPC1768 to use low speed(1.5 mbps).&lt;/P&gt;&lt;P&gt;I cannot find where this is configured if at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a register to change the USB speed to use low speed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 16:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-ac-as-USB-device-in-low-speed/m-p/1325571#M46195</guid>
      <dc:creator>enpingado</dc:creator>
      <dc:date>2021-08-18T16:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 ac as USB device in low speed</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-ac-as-USB-device-in-low-speed/m-p/1326698#M46221</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;enpingado,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There isn't a register.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If the USB host connected to LPC1768 is low speed, it will automatically change to low speed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 06:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-ac-as-USB-device-in-low-speed/m-p/1326698#M46221</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-20T06:55:25Z</dc:date>
    </item>
  </channel>
</rss>