<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Pin behavior during power up</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324735#M46184</link>
    <description>&lt;P&gt;Hey Alice,&lt;/P&gt;&lt;P&gt;The pin is being used as pwm, and with the following characteristics:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;const uint32_t port3_pin10_config = (&lt;BR /&gt;IOCON_PIO_FUNC3 |&lt;BR /&gt;IOCON_PIO_MODE_INACT | // I tried using the MODE_PULLDOWN function&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;IOCON_PIO_INPFILT_OFF |&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI&lt;BR /&gt;);&lt;BR /&gt;IOCON_PinMuxSet(IOCON, PORT3_IDX, PIN10_IDX, port3_pin10_config);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this way, the output of this pin is connected to the non-inverting port of an Ampop 741.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, RA.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 12:22:25 GMT</pubDate>
    <dc:creator>RodrigoEngComp</dc:creator>
    <dc:date>2021-08-17T12:22:25Z</dc:date>
    <item>
      <title>Pin behavior during power up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324009#M46172</link>
      <description>&lt;P&gt;I'm using a LPCXpresso54018 board and at the moment I energize two pin board has the behavior shown in the attached image, even if it's a short time, it affects the project's operation.&lt;/P&gt;&lt;P&gt;Is there anything I could do to avoid this high state?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for yout attention, regards.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Aug 2021 17:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324009#M46172</guid>
      <dc:creator>RodrigoEngComp</dc:creator>
      <dc:date>2021-08-16T17:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: Pin behavior during power up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324247#M46175</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;RodrigoEngComp,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;How about set pin MODE to Pull-down resistor enabled, or connect a external pull-down resistor with that pin.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 03:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324247#M46175</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-17T03:02:13Z</dc:date>
    </item>
    <item>
      <title>Re: Pin behavior during power up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324735#M46184</link>
      <description>&lt;P&gt;Hey Alice,&lt;/P&gt;&lt;P&gt;The pin is being used as pwm, and with the following characteristics:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;const uint32_t port3_pin10_config = (&lt;BR /&gt;IOCON_PIO_FUNC3 |&lt;BR /&gt;IOCON_PIO_MODE_INACT | // I tried using the MODE_PULLDOWN function&lt;BR /&gt;IOCON_PIO_INV_DI |&lt;BR /&gt;IOCON_PIO_DIGITAL_EN |&lt;BR /&gt;IOCON_PIO_INPFILT_OFF |&lt;BR /&gt;IOCON_PIO_SLEW_STANDARD |&lt;BR /&gt;IOCON_PIO_OPENDRAIN_DI&lt;BR /&gt;);&lt;BR /&gt;IOCON_PinMuxSet(IOCON, PORT3_IDX, PIN10_IDX, port3_pin10_config);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this way, the output of this pin is connected to the non-inverting port of an Ampop 741.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, RA.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 12:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1324735#M46184</guid>
      <dc:creator>RodrigoEngComp</dc:creator>
      <dc:date>2021-08-17T12:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: Pin behavior during power up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1326139#M46208</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;RodrigoEngComp,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This is a know issue, you can have a look at Errata:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;3.7 IOCON.1: On power-up the standard GPIO pins are not in high Z&lt;BR /&gt;mode by default&lt;BR /&gt;Introduction:&lt;BR /&gt;On the LPC540xx devices, on power-up, pins PIO0_0 to PIO0_31, PIO1_0 to PIO1_31,&lt;BR /&gt;PIO2_0 to PIO2_31, PIO3_0 to PIO3_31, PIO4_0 to PIO4_31, and PIO5_0 to PIO5_10&lt;BR /&gt;are in high Z mode by default (internal pull-up resistor and internal pull-down resistor are&lt;BR /&gt;disabled).&lt;BR /&gt;Problem:&lt;BR /&gt;Only on the LPC540xx device revision 0A (Boot ROM version 21.0), on power-up, pins&lt;BR /&gt;PIO0_0 to PIO0_31, PIO1_0 to PIO1_31, PIO2_0 to PIO2_31, PIO3_0 to PIO3_31,&lt;BR /&gt;PIO4_0 to PIO4_31, and PIO5_0 to PIO5_10 have the internal pull-ups enabled and are&lt;BR /&gt;not in high Z mode by default. Depending on the application, this can cause a higher&lt;BR /&gt;in-rush current and/or external circuits connected to the GPIO pins to work in an&lt;BR /&gt;unexpected manner.&lt;BR /&gt;Work-around:&lt;BR /&gt;This issue will be fixed in the next device revision 1B (Boot ROM version 21.1). Users&lt;BR /&gt;should carefully design their application and consider the impact of the GPIOs’ default&lt;BR /&gt;change from device revision 0A to device revision 1B. The user can identify the device&lt;BR /&gt;revisions by reading the DEVICE_ID1 register or by calling the Boot ROM version ISP/IAP&lt;BR /&gt;function.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 08:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Pin-behavior-during-power-up/m-p/1326139#M46208</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-08-19T08:49:25Z</dc:date>
    </item>
  </channel>
</rss>