<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1322478#M46152</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are seeing an issue on our microcontroller where after around 5-8 minutes the ADC reading is dropping ~100 ADC bits on 3 ADC channels being converted, when the input being sampled on the channel's is not fluctuating.&lt;/P&gt;&lt;P&gt;We are using the conversion sequence A to get the ADC results from the 3 channels every 1ms. At the end of the sequence interrupt, the software trigger is being used to loop back through and get the conversions again.&lt;/P&gt;&lt;P&gt;The ADC reference voltage is tied to the 3.3V supply - this voltage is also not changing.&lt;/P&gt;&lt;P&gt;I have attached the ADC config routine and sequence handler plus the raw ADC readings captured over an hour.&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Aug 2021 08:07:24 GMT</pubDate>
    <dc:creator>Heiser</dc:creator>
    <dc:date>2021-08-12T08:07:24Z</dc:date>
    <item>
      <title>LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1322478#M46152</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are seeing an issue on our microcontroller where after around 5-8 minutes the ADC reading is dropping ~100 ADC bits on 3 ADC channels being converted, when the input being sampled on the channel's is not fluctuating.&lt;/P&gt;&lt;P&gt;We are using the conversion sequence A to get the ADC results from the 3 channels every 1ms. At the end of the sequence interrupt, the software trigger is being used to loop back through and get the conversions again.&lt;/P&gt;&lt;P&gt;The ADC reference voltage is tied to the 3.3V supply - this voltage is also not changing.&lt;/P&gt;&lt;P&gt;I have attached the ADC config routine and sequence handler plus the raw ADC readings captured over an hour.&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 08:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1322478#M46152</guid>
      <dc:creator>Heiser</dc:creator>
      <dc:date>2021-08-12T08:07:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325105#M46187</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190153"&gt;@Heiser&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Looking at the configurations this looks good but this behavior seems strange. I have some questions about this:&lt;/P&gt;
&lt;P&gt;Could you let me know which SDK version are you using?&lt;/P&gt;
&lt;P&gt;Is there any event that could trigger this behavior in your application? Some signal that could introduce noise to the ADC capture?&lt;/P&gt;
&lt;P&gt;Is this present using any channel?&lt;/P&gt;
&lt;P&gt;As reference, in the following &lt;A href="https://www.nxp.com/docs/en/application-note/AN5250.pdf" target="_self"&gt;document&lt;/A&gt; there's some recommendations to improve the ADC measurement.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 02:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325105#M46187</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-08-18T02:52:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325297#M46191</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167559"&gt;@Alexis_A&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I think we have found the issue - one of the other ADC input channels had a negative voltage that would slowly drift down from 0V to ~-0.7V. When the channel measured around -0.3V this would then affect the ADC readings. It was repeatable with an external power supply.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Heiser&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 07:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325297#M46191</guid>
      <dc:creator>Heiser</dc:creator>
      <dc:date>2021-08-18T07:48:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325545#M46194</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190153"&gt;@Heiser&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm glad that you could find the issue.&lt;/P&gt;
&lt;P&gt;Only as a suggestion, to ensure the correct functionality of the MCU, the tolerance for negative voltage is limited to -0.5V.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 15:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54616J512BD208-ADC-conversion-reading-drooping-after-5-8/m-p/1325545#M46194</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-08-18T15:21:31Z</dc:date>
    </item>
  </channel>
</rss>