<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S16.h CAN0_BASE</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1319549#M46086</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp;:Thank you very much&lt;/P&gt;</description>
    <pubDate>Fri, 06 Aug 2021 07:24:11 GMT</pubDate>
    <dc:creator>RRD101</dc:creator>
    <dc:date>2021-08-06T07:24:11Z</dc:date>
    <item>
      <title>LPC55S16.h CAN0_BASE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1315175#M46003</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have a question. I installed the mcan interrupt transfer example from the SDK_2.x_LPC55S16 to try my first steps with this microcontroller and CAN.&lt;/P&gt;&lt;P&gt;Now i had a closer look on manual and sourcecode. I found the definition of the CAN0_BASE address in the file LPC55S16.h. But the address of &lt;STRIKE&gt;secure and&lt;/STRIKE&gt; nonsecure &lt;STRIKE&gt;are&lt;/STRIKE&gt;&amp;nbsp;is different as shown in page 14 of 1154 of the Usermanual. Now the question, whats wrong? Or have i misunderstood something, in terms of use?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 12:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1315175#M46003</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2021-07-29T12:10:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16.h CAN0_BASE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1316164#M46025</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well. &lt;BR /&gt;There seems to be an error in the table of the user manual. The base address of the Debug Mailbox and the CAN are switched. &lt;BR /&gt;The NS base address of the CAN is 0x4009_D000.&lt;BR /&gt;&lt;BR /&gt;I will report this issue to have it corrected in further versions.&lt;BR /&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 22:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1316164#M46025</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-07-30T22:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S16.h CAN0_BASE</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1319549#M46086</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp;:Thank you very much&lt;/P&gt;</description>
      <pubDate>Fri, 06 Aug 2021 07:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-h-CAN0-BASE/m-p/1319549#M46086</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2021-08-06T07:24:11Z</dc:date>
    </item>
  </channel>
</rss>