<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Communication between Lpc board and Dongle using FTDI</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1319273#M46077</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well. &lt;BR /&gt;Specifically, how are you planning to do the communication?&lt;BR /&gt;The MCU inside the dongle is acceded through UART and uses a USB to UART converter to make it possible. So using a device with a USB makes it possible to communicate with the dongle. &lt;BR /&gt;&lt;BR /&gt;I looking forward to your reply. IF you have more questions do not hesitate to ask me. &lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 05 Aug 2021 19:59:47 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2021-08-05T19:59:47Z</dc:date>
    <item>
      <title>Communication between Lpc board and Dongle using FTDI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1315187#M46005</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;Please, I want to ask if an LPC board can Communicate with Dongle OM15080-K32W using FTDI or other types of Dongles using FTDI?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 10:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1315187#M46005</guid>
      <dc:creator>aws1995</dc:creator>
      <dc:date>2021-07-29T10:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Lpc board and Dongle using FTDI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1319273#M46077</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well. &lt;BR /&gt;Specifically, how are you planning to do the communication?&lt;BR /&gt;The MCU inside the dongle is acceded through UART and uses a USB to UART converter to make it possible. So using a device with a USB makes it possible to communicate with the dongle. &lt;BR /&gt;&lt;BR /&gt;I looking forward to your reply. IF you have more questions do not hesitate to ask me. &lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 05 Aug 2021 19:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1319273#M46077</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-08-05T19:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Lpc board and Dongle using FTDI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1326024#M46200</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp; Hallo and thanks very much for the answer , i have used k32 with lpcXpresso55s69 Board , i would like to send data from my pc to lpc board then to forward this data to the k32 and then to recieve data from anoher k32 dongle , but the&amp;nbsp; problem is that lpc board support only uart with cdc , but as iknow that k32 support only ftdi and lpc borad do not support ftdi and i can not till now find a solution for that ?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 06:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1326024#M46200</guid>
      <dc:creator>aws1995</dc:creator>
      <dc:date>2021-08-19T06:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between Lpc board and Dongle using FTDI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1331995#M46339</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;You can use the USB full speed from the LPC55s69 to connect with the K32W. I suggest you contact FTDI to check if some modifications are needed for the USB CDC of the LPC55s69. Since both devices use USB communication is possible.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 22:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Communication-between-Lpc-board-and-Dongle-using-FTDI/m-p/1331995#M46339</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-08-30T22:58:09Z</dc:date>
    </item>
  </channel>
</rss>