<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: USB Downloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1311207#M45929</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188931" target="_self" aria-label="View Profile of apexman"&gt;&lt;SPAN class=""&gt;apexman&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;So do you want to use LPC54s018-evk? Pay attention, this chip doesn't have interflash.&lt;/P&gt;
&lt;P&gt;And you can use ISP- USB mode to download image with blhost:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jul 2021 09:45:41 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2021-07-21T09:45:41Z</dc:date>
    <item>
      <title>USB Downloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1310478#M45909</link>
      <description>&lt;P&gt;Hi, I was looking through the USB examples for the LPC54628 using the LPC54s018-EVK board and I am not sure exactly which one fits my needs. What I would like to do is send data using an external windows application to program the EEPROM and the internal Flash (512K). I am pretty sure it would not be considered "HID" or "Mass storage device(MSC)". The VCOM seemed like it would be similar, but wasn't sure if I could somehow convert it to be straight USB transfers to utilize the speed advantage. (of coarse finding an app to send data is another issue). I also looked at "lpcxpresso54628_rom_dev_cdc_bm" which seemed similar to the VCOM.&lt;BR /&gt;Any help guiding me towards an example would be appreciated.&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;Gennaro&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 15:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1310478#M45909</guid>
      <dc:creator>apexman</dc:creator>
      <dc:date>2021-07-20T15:36:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB Downloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1310757#M45919</link>
      <description>&lt;P&gt;The bottleneck is not going to be USB but the programming of the flash so bulk will not give you a big advantage. You could go DFU an re-use existing app on the host (dfu-static w/ windows' inbox driver WinUSB) or go MCUboot which uses HID (also Windows inbox driver).&amp;nbsp; This cuts down the dev on the host side with already available app and inbox kernel drivers if Windows is your host.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 23:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1310757#M45919</guid>
      <dc:creator>belmontbob59</dc:creator>
      <dc:date>2021-07-20T23:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB Downloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1311207#M45929</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188931" target="_self" aria-label="View Profile of apexman"&gt;&lt;SPAN class=""&gt;apexman&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;So do you want to use LPC54s018-evk? Pay attention, this chip doesn't have interflash.&lt;/P&gt;
&lt;P&gt;And you can use ISP- USB mode to download image with blhost:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Use-blhost-to-program-erase-LPC540xxM-LPC54S0xxM-flash/ta-p/1105629&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 09:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1311207#M45929</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-07-21T09:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: USB Downloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1435720#M48368</link>
      <description>&lt;P&gt;MCUBoot does not support USB ext flash programming via USB HID.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I m looking for a host side application as well which will program EVK 54S018 via USB HID.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DFU just programs the RAM so it's not really useful for production end&lt;/P&gt;</description>
      <pubDate>Tue, 29 Mar 2022 20:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Downloader/m-p/1435720#M48368</guid>
      <dc:creator>NVazquez</dc:creator>
      <dc:date>2022-03-29T20:16:55Z</dc:date>
    </item>
  </channel>
</rss>