<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Change device from LPC55S69 to LPC55S66 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310013#M45898</link>
    <description>&lt;P&gt;Hi, I have a project with LPC55S69JBD100 that works fine. But with the current supply chain issue, the part has a very long lead time. We are remaking the hardware to LPCS66JEV98. I changed the MCU on the project setting and the package changed as well. However, when I compile I still see the summary as:&lt;/P&gt;&lt;P&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt;PROGRAM_FLASH: 129432 B &lt;STRONG&gt;608&lt;/STRONG&gt; KB 20.79%&lt;BR /&gt;SRAM: 64336 B &lt;STRONG&gt;256&lt;/STRONG&gt; KB 24.54%&lt;BR /&gt;SRAM4: 0 GB 16 KB 0.00%&lt;BR /&gt;SRAMX: 0 GB 32 KB 0.00%&lt;BR /&gt;USB_RAM: 0 GB 16 KB 0.00%&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I did not change the memory setting, as it is using the LPC55xx.cfx as driver. But I would imaging I need to change the range of the flash and SRAM. I could not find where I should change the range to.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Huiji&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jul 2021 18:07:05 GMT</pubDate>
    <dc:creator>huijiwang</dc:creator>
    <dc:date>2021-07-19T18:07:05Z</dc:date>
    <item>
      <title>Change device from LPC55S69 to LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310013#M45898</link>
      <description>&lt;P&gt;Hi, I have a project with LPC55S69JBD100 that works fine. But with the current supply chain issue, the part has a very long lead time. We are remaking the hardware to LPCS66JEV98. I changed the MCU on the project setting and the package changed as well. However, when I compile I still see the summary as:&lt;/P&gt;&lt;P&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt;PROGRAM_FLASH: 129432 B &lt;STRONG&gt;608&lt;/STRONG&gt; KB 20.79%&lt;BR /&gt;SRAM: 64336 B &lt;STRONG&gt;256&lt;/STRONG&gt; KB 24.54%&lt;BR /&gt;SRAM4: 0 GB 16 KB 0.00%&lt;BR /&gt;SRAMX: 0 GB 32 KB 0.00%&lt;BR /&gt;USB_RAM: 0 GB 16 KB 0.00%&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I did not change the memory setting, as it is using the LPC55xx.cfx as driver. But I would imaging I need to change the range of the flash and SRAM. I could not find where I should change the range to.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Huiji&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 18:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310013#M45898</guid>
      <dc:creator>huijiwang</dc:creator>
      <dc:date>2021-07-19T18:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: Change device from LPC55S69 to LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310164#M45902</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189250" target="_self" aria-label="View Profile of huijiwang"&gt;&lt;SPAN class=""&gt;,&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Uncheck the "Preserve memory configuration" when chaneg MCU:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1626752141858.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150264iDB700B08775A8607/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1626752141858.png" alt="Alice_Yang_0-1626752141858.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Now based on your project, if it already lpc55s66, please first change back to lpc55s69, then try again.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 03:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310164#M45902</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-07-20T03:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: Change device from LPC55S69 to LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310509#M45910</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;wrote:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;Uncheck the "Preserve memory configuration" when chaneg MCU:&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks. That's a helpful hint. I finally have the proper memory configuration for my CPU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Heck, why is this option checked in the first place? It's trap, I gues, to make things complicated and befuddle the user.&amp;nbsp;I entered this dialog by right clicking the "MCU" entry in Project Explorer and selecting "Edit MCU". I assume that most of the times when changing MCUs you'd want to update the memory configuration.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 14:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310509#M45910</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2021-07-20T14:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: Change device from LPC55S69 to LPC55S66</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310631#M45913</link>
      <description>&lt;P&gt;Hi, Alice,&lt;/P&gt;&lt;P&gt;It works after I u&lt;SPAN&gt;ncheck the "Preserve memory configuration" when changing MCU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Huiji&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jul 2021 16:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Change-device-from-LPC55S69-to-LPC55S66/m-p/1310631#M45913</guid>
      <dc:creator>huijiwang</dc:creator>
      <dc:date>2021-07-20T16:57:27Z</dc:date>
    </item>
  </channel>
</rss>