<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSpeed of using LPC to write USB disk</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Speed-of-using-LPC-to-write-USB-disk/m-p/1304565#M45802</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;In my project, I need to export data to USB disk with the FatFs file system on lpc1788 platform. The real speed I tested was 400KB/s~450KB/s.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Official documents show that the USB speed can reach 12Mb/s(1.5MB/s).&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The USB device controller on the LPC178x/177x enables full-speed (12 Mb/s) data&lt;BR /&gt;exchange with a USB host controller.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Therefore, my question is, what is the maximum speed that lpc1788 can export data to USB disk, and how can I improve the speed?&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jul 2021 07:39:14 GMT</pubDate>
    <dc:creator>canheting</dc:creator>
    <dc:date>2021-07-08T07:39:14Z</dc:date>
    <item>
      <title>Speed of using LPC to write USB disk</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Speed-of-using-LPC-to-write-USB-disk/m-p/1304565#M45802</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;In my project, I need to export data to USB disk with the FatFs file system on lpc1788 platform. The real speed I tested was 400KB/s~450KB/s.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Official documents show that the USB speed can reach 12Mb/s(1.5MB/s).&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The USB device controller on the LPC178x/177x enables full-speed (12 Mb/s) data&lt;BR /&gt;exchange with a USB host controller.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Therefore, my question is, what is the maximum speed that lpc1788 can export data to USB disk, and how can I improve the speed?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 07:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Speed-of-using-LPC-to-write-USB-disk/m-p/1304565#M45802</guid>
      <dc:creator>canheting</dc:creator>
      <dc:date>2021-07-08T07:39:14Z</dc:date>
    </item>
    <item>
      <title>Re: Speed of using LPC to write USB disk</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Speed-of-using-LPC-to-write-USB-disk/m-p/1304660#M45804</link>
      <description>&lt;P&gt;Hi, Geng,&lt;/P&gt;
&lt;P&gt;I think the Flash erasing/programing dominate the usb disk speed rather than the USB transfer speed.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 09:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Speed-of-using-LPC-to-write-USB-disk/m-p/1304660#M45804</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-07-08T09:11:57Z</dc:date>
    </item>
  </channel>
</rss>