<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC-LinkII UART baud</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-LinkII-UART-baud/m-p/1304482#M45799</link>
    <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I am confused at LPC Link II UART baud.&lt;/P&gt;&lt;P&gt;I got an example code from LPC Open. There's an example code. It's named "periph_uart". I upload it to my board. And it seems can not work. Only receive garbled. I tried MB3232I and Arduino. Both of them received&amp;nbsp;&lt;SPAN&gt;garbled. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But if I change the baud rate to 9600. (Example code is 115200) They can receive correctly. Does this means this board can only send UART with baud 9600? Or where should I check to speed up the baud rate?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jul 2021 05:35:51 GMT</pubDate>
    <dc:creator>JiaAn</dc:creator>
    <dc:date>2021-07-08T05:35:51Z</dc:date>
    <item>
      <title>LPC-LinkII UART baud</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-LinkII-UART-baud/m-p/1304482#M45799</link>
      <description>&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;I am confused at LPC Link II UART baud.&lt;/P&gt;&lt;P&gt;I got an example code from LPC Open. There's an example code. It's named "periph_uart". I upload it to my board. And it seems can not work. Only receive garbled. I tried MB3232I and Arduino. Both of them received&amp;nbsp;&lt;SPAN&gt;garbled. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But if I change the baud rate to 9600. (Example code is 115200) They can receive correctly. Does this means this board can only send UART with baud 9600? Or where should I check to speed up the baud rate?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 05:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-LinkII-UART-baud/m-p/1304482#M45799</guid>
      <dc:creator>JiaAn</dc:creator>
      <dc:date>2021-07-08T05:35:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-LinkII UART baud</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-LinkII-UART-baud/m-p/1305374#M45827</link>
      <description>&lt;P&gt;Hi JiaAn&lt;/P&gt;
&lt;P&gt;Which demo board do you work with? Could you send me a link of it? I will test it on my side.&lt;/P&gt;
&lt;P&gt;Meanwhile, could you please also test other demos included in LPCOpen package?&lt;/P&gt;
&lt;P&gt;How does it work on other computer?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 09 Jul 2021 10:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-LinkII-UART-baud/m-p/1305374#M45827</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-07-09T10:06:14Z</dc:date>
    </item>
  </channel>
</rss>