<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 About internal ROM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-internal-ROM/m-p/1303661#M45775</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Does the built-in ROM cause the data to be rewritten without permission?&lt;BR /&gt;When a programming file is written, mounted on a board, and then inspected, a phenomenon occurs in which it is rarely rewritten and does not work.&lt;BR /&gt;I don't know what caused it.&lt;BR /&gt;Can it be caused by any settings or external factors?&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 06:37:57 GMT</pubDate>
    <dc:creator>taka01</dc:creator>
    <dc:date>2021-07-07T06:37:57Z</dc:date>
    <item>
      <title>About internal ROM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-internal-ROM/m-p/1303661#M45775</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Does the built-in ROM cause the data to be rewritten without permission?&lt;BR /&gt;When a programming file is written, mounted on a board, and then inspected, a phenomenon occurs in which it is rarely rewritten and does not work.&lt;BR /&gt;I don't know what caused it.&lt;BR /&gt;Can it be caused by any settings or external factors?&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 06:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-internal-ROM/m-p/1303661#M45775</guid>
      <dc:creator>taka01</dc:creator>
      <dc:date>2021-07-07T06:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: About internal ROM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-internal-ROM/m-p/1303801#M45782</link>
      <description>&lt;P&gt;LPC43 BootRom doesn't program without permission.&lt;/P&gt;
&lt;P&gt;What tool do you use to program board? How can I reproduce your issue?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jennie&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 08:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-internal-ROM/m-p/1303801#M45782</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-07-07T08:48:27Z</dc:date>
    </item>
  </channel>
</rss>