<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCAN LPC55S1X in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1301127#M45708</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ok, and how would I cut the transmission, I mean, I'm using the MCAN_TransferSendNonBlocking function, and it never stops, I just want to send the data once and cut the transmission, how should I do it, that the transmission doesn't stop means that it's being done wrong?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jul 2021 11:57:05 GMT</pubDate>
    <dc:creator>Nadia</dc:creator>
    <dc:date>2021-07-01T11:57:05Z</dc:date>
    <item>
      <title>MCAN LPC55S1X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1293172#M45491</link>
      <description>&lt;P&gt;Hello to all.&lt;BR /&gt;I am trying to make a communication from the CAN protocol. To do this, as well as reading the relevant documentation for both the micro and the communications protocol, I have uploaded an example to see how it works. It is a bit confusing for me, could someone explain me in which part of the example code I can access the data that is sent at the beginning of the frame according to the CAN protocol? Also could you tell me in which part of the code I can access the ID identifier data according to the CAN protocol?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you very much.&lt;BR /&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 09:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1293172#M45491</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-06-16T09:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCAN LPC55S1X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1294291#M45523</link>
      <description>&lt;P&gt;Hi Nadia,&lt;/P&gt;
&lt;P&gt;By the data in the beginning on the frame do you mean identifier as well?&lt;/P&gt;
&lt;P class="lia-align-center"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FelipeGarcia_1-1623966341968.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147375iD61F29C9B079A173/image-size/large?v=v2&amp;amp;px=999" role="button" title="FelipeGarcia_1-1623966341968.png" alt="FelipeGarcia_1-1623966341968.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This information is contained in the txFrame and rxFrame structures of the MCAN examples.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 21:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1294291#M45523</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-06-17T21:46:16Z</dc:date>
    </item>
    <item>
      <title>Re: MCAN LPC55S1X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1301127#M45708</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167536"&gt;@FelipeGarcia&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ok, and how would I cut the transmission, I mean, I'm using the MCAN_TransferSendNonBlocking function, and it never stops, I just want to send the data once and cut the transmission, how should I do it, that the transmission doesn't stop means that it's being done wrong?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jul 2021 11:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1301127#M45708</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-07-01T11:57:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCAN LPC55S1X</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1305032#M45808</link>
      <description>&lt;P&gt;Hi Nadia,&lt;/P&gt;
&lt;P&gt;This is because the transmission is not being completed correctly, therefore, MCAN module generates retransmission. Please check description below from the UM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_1-1625785042870.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/149306i8F834456BA55C062/image-size/medium?v=v2&amp;amp;px=400" role="button" title="FelipeGarcia_1-1625785042870.png" alt="FelipeGarcia_1-1625785042870.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jul 2021 22:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCAN-LPC55S1X/m-p/1305032#M45808</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-07-08T22:57:50Z</dc:date>
    </item>
  </channel>
</rss>