<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using FAIM for Hi-Z port pin while LPC844 held in reset in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-FAIM-for-Hi-Z-port-pin-while-LPC844-held-in-reset/m-p/1299627#M45682</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;If the LPC844 processor is configured so that a port pin is configured using the FAIM for Hi-Z , (No pull-up, no pull-down).&amp;nbsp; If the Reset pin is HELD low, while held low , does the pin state match that as for the FAIM config.&lt;/P&gt;&lt;P&gt;I have a situation, with are external volt-supervisor, due to possibility of slow ramp supply volts.&lt;/P&gt;&lt;P&gt;I don't want the port pin to source current from the weak pull-up, during Reset Low.&lt;/P&gt;&lt;P&gt;My code puts pin state o/p low as soon a it can. Using FAIM I can have hi-z pin state, but user manual seems to suggest it only kicks in AFTER Reset, not while Reset is active.&lt;/P&gt;&lt;P&gt;Testing seems to show that the pin is hi-z, but can you please confim.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 29 Jun 2021 10:33:22 GMT</pubDate>
    <dc:creator>mike_hackett</dc:creator>
    <dc:date>2021-06-29T10:33:22Z</dc:date>
    <item>
      <title>Using FAIM for Hi-Z port pin while LPC844 held in reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-FAIM-for-Hi-Z-port-pin-while-LPC844-held-in-reset/m-p/1299627#M45682</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;If the LPC844 processor is configured so that a port pin is configured using the FAIM for Hi-Z , (No pull-up, no pull-down).&amp;nbsp; If the Reset pin is HELD low, while held low , does the pin state match that as for the FAIM config.&lt;/P&gt;&lt;P&gt;I have a situation, with are external volt-supervisor, due to possibility of slow ramp supply volts.&lt;/P&gt;&lt;P&gt;I don't want the port pin to source current from the weak pull-up, during Reset Low.&lt;/P&gt;&lt;P&gt;My code puts pin state o/p low as soon a it can. Using FAIM I can have hi-z pin state, but user manual seems to suggest it only kicks in AFTER Reset, not while Reset is active.&lt;/P&gt;&lt;P&gt;Testing seems to show that the pin is hi-z, but can you please confim.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 10:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-FAIM-for-Hi-Z-port-pin-while-LPC844-held-in-reset/m-p/1299627#M45682</guid>
      <dc:creator>mike_hackett</dc:creator>
      <dc:date>2021-06-29T10:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: Using FAIM for Hi-Z port pin while LPC844 held in reset</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-FAIM-for-Hi-Z-port-pin-while-LPC844-held-in-reset/m-p/1301234#M45709</link>
      <description>&lt;P&gt;Hi Mike&lt;/P&gt;
&lt;P&gt;FAIM is for MCU initial configuration AFTER reset. The initialization includes:&lt;BR /&gt;− FRO clock frequency&lt;BR /&gt;− Pin configuration with pull ups, pull downs, and tri state&lt;BR /&gt;− SWD&lt;BR /&gt;− ISP interface for programming and ISP pins&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;One reset cycle&lt;/STRONG&gt; is needed to make this initialization take effect. And because FAIM programming voltage range is 3.0 V ≤ Vdd ≤ 3.6 V. So during ramup that Vdd is lower than 3.3v, FAIM setting can't take effect.&lt;/P&gt;
&lt;P&gt;We don't have official data of pin status during RESET pin low.&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jul 2021 14:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-FAIM-for-Hi-Z-port-pin-while-LPC844-held-in-reset/m-p/1301234#M45709</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-07-01T14:27:13Z</dc:date>
    </item>
  </channel>
</rss>