<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC802 power consumption</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1296599#M45593</link>
    <description>&lt;P&gt;In addition, Below are necessary for Idd measurement:&lt;/P&gt;
&lt;P&gt;1. IDD measurements were performed with all pins configured as GPIO outputs driven LOW and pull-up resistors disabled.&lt;BR /&gt;2.&amp;nbsp; FRO enabled.&lt;BR /&gt;3. BOD disabled.&lt;BR /&gt;4.&amp;nbsp; All peripherals disabled in the SYSAHBCLKCTRL register. Peripheral clocks disabled in system configuration block.&lt;BR /&gt;5,&amp;nbsp; All oscillators and analog blocks turned off.&lt;BR /&gt;6.&amp;nbsp; WAKEUP function pin pulled HIGH externally.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 06:55:11 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-06-23T06:55:11Z</dc:date>
    <item>
      <title>LPC802 power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1295037#M45543</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I get a OM40000&amp;nbsp;RevA (LPC802) EVB, and trying to get the the power&amp;nbsp;consumption about it.&lt;BR /&gt;I install&amp;nbsp;MCUXpressoIDE v11.3.1, SDK v2.9.0.&lt;BR /&gt;Import project&amp;nbsp;power_mode_switch from sdk, and change code as attach file.&lt;BR /&gt;Remove JP1 jumper, connect a&amp;nbsp;ammeter at JP1, flash code and repower EVB.&lt;BR /&gt;I got about 139uA after 10s.&lt;BR /&gt;Is this right? For me, it is to high. (I need 20~30uA in my product)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 00:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1295037#M45543</guid>
      <dc:creator>frank-lin-Sunon</dc:creator>
      <dc:date>2021-06-21T00:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1295711#M45570</link>
      <description>&lt;P&gt;After remove&amp;nbsp;LED&amp;nbsp;daughter&amp;nbsp;board, i could get about 50uA.&lt;BR /&gt;But If i add GPIO init, it will increase to 110uA. Is this&amp;nbsp;correct?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 01:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1295711#M45570</guid>
      <dc:creator>frank-lin-Sunon</dc:creator>
      <dc:date>2021-06-22T01:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1296402#M45590</link>
      <description>&lt;P&gt;I found the problem.&lt;BR /&gt;All pin will pull-up after reset, i need to disable pull-up.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 00:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1296402#M45590</guid>
      <dc:creator>frank-lin-Sunon</dc:creator>
      <dc:date>2021-06-23T00:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC802 power consumption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1296599#M45593</link>
      <description>&lt;P&gt;In addition, Below are necessary for Idd measurement:&lt;/P&gt;
&lt;P&gt;1. IDD measurements were performed with all pins configured as GPIO outputs driven LOW and pull-up resistors disabled.&lt;BR /&gt;2.&amp;nbsp; FRO enabled.&lt;BR /&gt;3. BOD disabled.&lt;BR /&gt;4.&amp;nbsp; All peripherals disabled in the SYSAHBCLKCTRL register. Peripheral clocks disabled in system configuration block.&lt;BR /&gt;5,&amp;nbsp; All oscillators and analog blocks turned off.&lt;BR /&gt;6.&amp;nbsp; WAKEUP function pin pulled HIGH externally.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 06:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC802-power-consumption/m-p/1296599#M45593</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-06-23T06:55:11Z</dc:date>
    </item>
  </channel>
</rss>