<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックADC Sampling Rate (LPCSS06-EVK)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sampling-Rate-LPCSS06-EVK/m-p/1296366#M45588</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using the on-board ADC to take in a sinusoidal voltage input at 1kHz. I have run into an issue though: the sampling rate is not high enough. I see in the datasheet that the chip supports up to 2 Msamples/second; however, my ADC is not producing the accurate results that I want. I am wanting to know how to change these settings to where I can achieve the highest accuracy possible. I have tried to change the ADC clock settings in the clocks diagram tab but to no avail. I have attached the file with the ADC values (the values that should represent a sine wave) so you can see my issue.&lt;/P&gt;&lt;P&gt;If someone could help, I would greatly appreciate it.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Jun 2021 21:35:14 GMT</pubDate>
    <dc:creator>caden013</dc:creator>
    <dc:date>2021-06-22T21:35:14Z</dc:date>
    <item>
      <title>ADC Sampling Rate (LPCSS06-EVK)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sampling-Rate-LPCSS06-EVK/m-p/1296366#M45588</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using the on-board ADC to take in a sinusoidal voltage input at 1kHz. I have run into an issue though: the sampling rate is not high enough. I see in the datasheet that the chip supports up to 2 Msamples/second; however, my ADC is not producing the accurate results that I want. I am wanting to know how to change these settings to where I can achieve the highest accuracy possible. I have tried to change the ADC clock settings in the clocks diagram tab but to no avail. I have attached the file with the ADC values (the values that should represent a sine wave) so you can see my issue.&lt;/P&gt;&lt;P&gt;If someone could help, I would greatly appreciate it.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 21:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sampling-Rate-LPCSS06-EVK/m-p/1296366#M45588</guid>
      <dc:creator>caden013</dc:creator>
      <dc:date>2021-06-22T21:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sampling Rate (LPCSS06-EVK)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sampling-Rate-LPCSS06-EVK/m-p/1296514#M45591</link>
      <description>&lt;P&gt;I would start with reading the ADC section of the user manual.&lt;/P&gt;&lt;P&gt;The sampling frequency is determined by your method of triggering a conversion.&lt;/P&gt;&lt;P&gt;I am using a timer in one of my applications (for the LPC54628):&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;adcConvSeqConfigStruct.triggerMask = ADC_TRG_CTIMER0_MAT3;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Enabling/running the timer will start the sampling.&lt;/P&gt;&lt;P&gt;The ADC clock determines only the ADC-internal timing, e.g. sampling and conversion times.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 05:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sampling-Rate-LPCSS06-EVK/m-p/1296514#M45591</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-06-23T05:24:13Z</dc:date>
    </item>
  </channel>
</rss>