<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SWM on LPC845: connecting to hardware with clocks disabled in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1295029#M45542</link>
    <description>&lt;P&gt;Hi Gustavo, thank you for looking into this.&lt;/P&gt;&lt;P&gt;I looked into the USART section of UM11029 and it says&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Configure the USARTs for receiving and transmitting data:&lt;BR /&gt;• In the SYSAHBCLKCTRL register, set bit 14 to 16, bit 30, and 31 (Table 146) to&lt;BR /&gt;enable the clock to the register interface.&lt;/P&gt;&lt;P&gt;...&lt;BR /&gt;• Configure the USART pin functions through the switch matrix.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Which makes sense to me. I realize UM11029 is a large document, probably it was just a mistake in the SWM section.&lt;/P&gt;</description>
    <pubDate>Sun, 20 Jun 2021 20:40:15 GMT</pubDate>
    <dc:creator>loudpotato</dc:creator>
    <dc:date>2021-06-20T20:40:15Z</dc:date>
    <item>
      <title>SWM on LPC845: connecting to hardware with clocks disabled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1291687#M45451</link>
      <description>&lt;P&gt;Hi. I am looking into configuring pins on LPC845, SWM documentation says:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Before activating a peripheral or enabling its interrupt, use the switch matrix to connect the&lt;BR /&gt;peripheral to external pins.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Let's say I assign U0_TXD to PIO0_0 but leave UART0 without clocks in SYSAHBCLKCTRL0. What state of the PIO0_0 will be (driven high, hi-z, something else)?&lt;/P&gt;</description>
      <pubDate>Sun, 13 Jun 2021 22:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1291687#M45451</guid>
      <dc:creator>loudpotato</dc:creator>
      <dc:date>2021-06-13T22:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: SWM on LPC845: connecting to hardware with clocks disabled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1293550#M45497</link>
      <description>&lt;P&gt;Hello Loudpotato,&lt;/P&gt;
&lt;P&gt;The PIO0_0 state out of reset would be Input, internal pull-up enabled.&lt;/P&gt;
&lt;P&gt;Once you have configured it as U0_TXD it would be an output, as this signal is the transmitter output. But the state would depend on the UART module, and I couldn’t find a known default state when the UART module has its clock disabled.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 19:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1293550#M45497</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-06-16T19:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: SWM on LPC845: connecting to hardware with clocks disabled</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1295029#M45542</link>
      <description>&lt;P&gt;Hi Gustavo, thank you for looking into this.&lt;/P&gt;&lt;P&gt;I looked into the USART section of UM11029 and it says&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Configure the USARTs for receiving and transmitting data:&lt;BR /&gt;• In the SYSAHBCLKCTRL register, set bit 14 to 16, bit 30, and 31 (Table 146) to&lt;BR /&gt;enable the clock to the register interface.&lt;/P&gt;&lt;P&gt;...&lt;BR /&gt;• Configure the USART pin functions through the switch matrix.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Which makes sense to me. I realize UM11029 is a large document, probably it was just a mistake in the SWM section.&lt;/P&gt;</description>
      <pubDate>Sun, 20 Jun 2021 20:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SWM-on-LPC845-connecting-to-hardware-with-clocks-disabled/m-p/1295029#M45542</guid>
      <dc:creator>loudpotato</dc:creator>
      <dc:date>2021-06-20T20:40:15Z</dc:date>
    </item>
  </channel>
</rss>