<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Setting of DEBUG_LOCK_EN on LPC55S69 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1294230#M45519</link>
    <description>&lt;P&gt;Hi Marvin,&lt;/P&gt;
&lt;P&gt;So you would like to set 0xA to the register? This means that you enable write access to security registers.&lt;/P&gt;
&lt;P&gt;I also read value when starting a new project and I also read 0x5 value. I am going to contact internal team to see if they have some feedback about this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_0-1623948685415.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147367i88698DB60E7641ED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="FelipeGarcia_0-1623948685415.png" alt="FelipeGarcia_0-1623948685415.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;FelipeGarcia_0-1623948685415.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
    <pubDate>Thu, 17 Jun 2021 16:51:39 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2021-06-17T16:51:39Z</dc:date>
    <item>
      <title>Setting of DEBUG_LOCK_EN on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1291801#M45453</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to disable the debug- as well as the programming- (SWD) interfaces on our custom LPC55S69 board&amp;nbsp; in order to secure our IP.&lt;/P&gt;&lt;P&gt;While reading the DEBUG_FEATURES and DEBUG_FEATURES_DP returns as expected, reading DEBUG_LOCK_EN resulted in 0x5, which means all write accesses to the debug and programming registers are permitted and ignored.&lt;/P&gt;&lt;P&gt;I was wondering, where the write lock is set to 0x5 in the examples. I couldn't find the line.&lt;/P&gt;&lt;P&gt;Hope you can help me with this. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help and all the best,&lt;BR /&gt;marvin&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 08:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1291801#M45453</guid>
      <dc:creator>__marvin__</dc:creator>
      <dc:date>2021-06-14T08:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: Setting of DEBUG_LOCK_EN on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1294230#M45519</link>
      <description>&lt;P&gt;Hi Marvin,&lt;/P&gt;
&lt;P&gt;So you would like to set 0xA to the register? This means that you enable write access to security registers.&lt;/P&gt;
&lt;P&gt;I also read value when starting a new project and I also read 0x5 value. I am going to contact internal team to see if they have some feedback about this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="FelipeGarcia_0-1623948685415.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147367i88698DB60E7641ED/image-size/medium?v=v2&amp;amp;px=400" role="button" title="FelipeGarcia_0-1623948685415.png" alt="FelipeGarcia_0-1623948685415.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;FelipeGarcia_0-1623948685415.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 16:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1294230#M45519</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-06-17T16:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: Setting of DEBUG_LOCK_EN on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1294280#M45521</link>
      <description>&lt;P&gt;Hi Felipe,&lt;/P&gt;&lt;P&gt;thanks for verifying this. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;If there should be a response, please let me know.&lt;/P&gt;&lt;P&gt;All the best,&lt;BR /&gt;marvin&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 20:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1294280#M45521</guid>
      <dc:creator>__marvin__</dc:creator>
      <dc:date>2021-06-17T20:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: Setting of DEBUG_LOCK_EN on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1295658#M45569</link>
      <description>&lt;P&gt;Hi Marvin,&lt;/P&gt;
&lt;P&gt;I have received confirmation from internal team. Please check it below.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;EM&gt;After POR, the related six registers&amp;nbsp;(CPU0_DEBUG_FEATURES,CPU1_DEBUG_FEATURES…) will be configured based on the PFR data in the CFPA DCFG_CC_SOCU_NS_PIN and &amp;nbsp;DCFG_CC_SOCU_NS_DFLT (0x9de20 – 0x9de27), and CMPA DCFG_CC_SOCU_PIN and DCFG_CC_SOCU_DFLT (0x9e410 – 0x9e41b), and then&amp;nbsp;the ROM will set DEBUG_LOCK_EN to 0x5.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;EM&gt;You can refer to AN13037(&lt;A href="https://www.nxp.com/docs/en/application-note/AN13037.pdf" target="_blank"&gt;LPC55Sxx Debug Authentication&lt;/A&gt;) for details.&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 21:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1295658#M45569</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-06-21T21:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: Setting of DEBUG_LOCK_EN on LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1296273#M45586</link>
      <description>&lt;P&gt;Thank you so much! This really helped me a lot. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jun 2021 16:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Setting-of-DEBUG-LOCK-EN-on-LPC55S69/m-p/1296273#M45586</guid>
      <dc:creator>__marvin__</dc:creator>
      <dc:date>2021-06-22T16:03:01Z</dc:date>
    </item>
  </channel>
</rss>